Hi Anshuman
Anshuman Srinivasan said: I would suggest you still try to set your configuration register at 0x72 to 0xDCFE
What is value of ADC_CCS_CFG for this test?
When 0x72=0xDCFE and ADC_CCS_CFG = 0x040F, actually the sample sequence is VDAC1-> ... ->VDAC4…
Part Number: AMC60804 I have a question regarding AMC60804’s Supplies connection for following operations,
I2C SDA & SCL voltage = 2.5V
ADC full scale = 2.5V
VDAC full scale = 2.5V
/RESET = 2.5V
/PWDWN = 2.5V
/LDAC = 2.5V
Do I connect VIO to…
Part Number: AMC60804 I downloaded AMC60804 datasheet online,
https://www.ti.com/lit/ds/symlink/amc60804.pdf?ts=1662991799586
but it is very brief not much helpful.
We already have this chip onboard but the designer has left company.
Please help with…
Part Number: AMC60804 Other Parts Discussed in Thread: AMC60304 Hi Sir,
may we know the pin define of AMC60804 and AMC60304 is the same? because seem is same package and body size.
can AMC60804 directly replace AMC60304?
Part Number: AMC60804 Hi TI Team,
I need quick verification on below point for my design,
1) D oes I2C logic levels follows VIO Voltage level in AMC60804 ?
Due to change in design, I need to switch I2C from 3.3V to 2.5V , make it compatible with new Microprocessor…
Part Number: AMC60804 Hi all,
Please help to check my customer's design about AMC60804. I can't get full version datasheet / EVM user guide so I can't check it directly. Thanks for your kindly help.
Best regards,
Gary Teng
Part Number: AMC60804 Hi
I have few question as below
1.Could IDAC1~IDAC4 be connected together and let the current output reach 600mA ?
2.If i don't use VCC/VSS/VDAC , could these pin be connected to GND?
Part Number: AMC60804 Hi Expert
Could I use -1.8V/GND for VDAC supply? If I only need -1.5V to 0V output range.
Just want to get higher efficiency for whole system. With -1.8V supply, I can use a DCDC to translate 3.3V to -1.8V, so that to save more linear…
Part Number: AMC60804 How to deal with the Internal 2.5-V reference of amc60804 when it is not used? Need to connect capacitor or float processing! thank you