Part Number: ATL431 Other Parts Discussed in Thread: TL431 Hello,
there seems still to be the issue with start-up response of the ATL431B model which is different to the start-up response shown in the datasheet. The issue was also part of a discussion about…
Part Number: ATL431 Other Parts Discussed in Thread: TL431 , Hi Team,
We would like to use TL431 calc tool. We have several questions about how to use this tool.
1) Is it no problem to apply TL431 calc tool for ATL431? 2) Is my thought below correct because…
Part Number: ATL431 Hello Expert,
I am planning to use ATL431BQDBZR for an SMPS of 5W 20V output and get get confused at designing the value of resistor and capacitor marked in the below figure. Is there any document/article available for the proper design…
Part Number: ATL431 Hi Team,
Example values of Feedback resistor(R1 and R2) are 10kΩ in the data sheet.
1) Is it OK to R1=33kΩ and R2=100kΩ? 2) Do R1 and R2 have upper limit and lower limit? 3) How should we decide which several hundred…
Part Number: ATL431 Other Parts Discussed in Thread: , TL431LI Hi,
I'm considering an ATL431 with Vka=-10V and I'm looking into the stability regions. On Figure16 it looks like the device is stable with 10uF @ 1mA but Figure 20 then seems to imply this…
Part Number: ATL431 Hi team,
Let me confirm definition of CKA which is shown at some figures such as figure 14~18.
Does it mean external capacitor connected between Cathode and Anode?
Is it okay to assume CKA is same as CL of figure32?
Best regards…
Part Number: ATL431 Hi team,
My customer want to use ATL43X to design a adjustable regulator. He wants to get max limit current (10mA). Can our chips support this design? If we can, how to design?
Thanks a lot!
BR
Gust
Part Number: ATL431 Other Parts Discussed in Thread: ATL432 , , Hello guys,
One of my customers considering using ATL431 or ATL432 for their next products.
They have the following questions. Could you please give me your reply?
Q1. Fiqure 19 on page 8 of…