Part Number: AWRL1432BOOST-BSD Other Parts Discussed in Thread: AWRL1432
Tool/software:
Hi,
In the radar_toolbox_2_10_00_04\source\ti\examples\ADAS\awrl1432_entry_level_blind_spot_detection\prebuilt_binaries, we can only get the binary file adas_bsd_demo…
Part Number: AWRL1432BOOST Dear All, I am checking example code "motion_and_presence_detection" on AWRL1432BOOST. In this example, I want to analyze the continuous radar spectrum after multiple chirps. In other words, I would like to do followings…
Part Number: AWRL1432BOOSTAWRL1432BOOST Hello, I am trying to get raw data from AWRL1432BOOST using DCA1000 ;
BUT, ,
I want know how to set S1 and S2 toggle swich to get raw data .
which step to step set mmwaveStudio?
thank you very much!
Part Number: AWRL1432BOOST Other Parts Discussed in Thread: UNIFLASH
Hello I am a novice for TI's CCS environment. I am trying to check board status, such as how to flash binary, what I flashed...etc. I have question as below.
Q1. I think too basic question…
Part Number: AWRL1432BOOST Other Parts Discussed in Thread: UNIFLASH hello, I am trying to run the "motion_and_presence_detection_demo" example on the AWRL1432Boost board. I can successfully check the behavior of the example by sending the configuration…
Part Number: AWRL1432 Hi,
My customer wants to modify AWRL1432BOOST to test BOM Opt mode. They removed the U19 and L5, but the system seems not work normally.
Must customer remove the capacities which are connected to VNWA?
What else are missing to make…
Part Number: AWRL1432BOOST Other Parts Discussed in Thread: AWRL1432
Hi,
I use mmwave studio+DCA1000 capture adc data. Radar Target Simulator set a target at 20m and 5m/s, but after studio post processing, target velocity is not 5m/s, why is this happening…
Part Number: AWRL1432BOOST Other Parts Discussed in Thread: AWRL1432 Hi,
I find HWA CFAR Engine in AWRL1432 with local max check, so my question is why not config CFAR engine with peak enable directly, but search peak in Post Processing?
parking_9m.cfg…
Part Number: AWRL1432BOOST Hi,
I want to config slow-fast frame using mmwave studio4.1.0.5, what should i do?
TRANSLATE with x
English
Arabic
Hebrew
Polish
Bulgarian
Hindi
Portuguese
Catalan
Hmong Daw
Romanian
Chinese Simplified
Hunga…