Part Number: AWRL1432BOOST Other Parts Discussed in Thread: SYSCONFIG hello, I am trying to flash basic example binary to AWRL1432BOOST eval board and then check it working. I could find example binary from sdk folder in "\MMWAVE_L_SDK_05_04_00_01\examples…
Part Number: AWRL1432BOOST Other Parts Discussed in Thread: MMWAVE-L-SDK , AWRL1432 Hello,
I just received AWRL1432BOOST Eval-board and I tried loading the example code with ccs via connecting to usb.
But hard fault is happened.Could somebody give me advice…
Part Number: AWRL1432BOOST Hello, in MMWAVE_L_SDK_05_04_00_01 DopplerProc DPU, i dont understand the format about M0( circled in green line), can you explain it ? Thanks!
TRANSLATE with x
English
Arabic
Hebrew
Polish
Bulgarian
Hindi
Portugues…
Part Number: AWRL1432BOOST Hi experts,
In the following link: frameCfg numOfChirpsAccum parameter, I have known the information that if I configure the frameCfg 128 2 4000 1 100 0 , the chirps that will be processed will be 128/2 = 64 chirps.
I have two questions…
Part Number: AWRL1432BOOST Other Parts Discussed in Thread: AWRL1432 Hi,
My customer try to test the AWRL1432 EVM antenna pattern to compare their result with the one in EVM user guide, they want to know about the test corner reflector size used to get…
Part Number: AWRL1432BOOST Other Parts Discussed in Thread: AWRL1432
Hello TI team,
I´m using a LIN driver which uses the standalone UART/SCI peripheral and not the LIN peripheral so I´m not able bring up the LIN communication since the LIN T…
Part Number: AWRL1432BOOST
Hi Experts
Customer is using AWRL1432EVM in CW mode to test the phase noise of our device.
They are sending sensor start several times in exact same power cycle. and find the peak power varies about 1.5dB.
Why the peak pow…
Part Number: AWRL1432BOOST Other Parts Discussed in Thread: IWRL6432 , AWRL1432
Cortex_M4_0: Can't Run Target CPU: (Error -1268 @ 0x1090001) Device is locked up in Hard Fault or in NMI. Reset the device, and retry the operation. If error persists, confirm…
Part Number: AWRL1432BOOST Hi team,
I'm testing the CAN-FD of 1432 and run mcan_external_read_write.release.appimage on boost evm. But there is no output.
The UART output is above, it seems this app can't be finished. Please help find the reason…