Part Number: BQ2002C Other Parts Discussed in Thread: BQ2002F , BQ25303J , BQ25302 , BQ25616 , BQ25300 , BQ25172 , BQ2002 Hello team, The customer has a question. The customer is considering to evaluate BQ2002C. BQ2002C/E datasheet says the following in Synchronized…
Other Parts Discussed in Thread: BQ2002F , BQ2002C Dear TI support staff,
I'm designing a single Ni-MH 9V battery charger and after searching and comparing PNs I came across the BQ2002F which seems to fit the design specs and budget. However I'm not sure…
Hi, In the last months I introduce a Bq2002F in my design to charge NiMH batteries (4cells; TM=mid and C/2 rate). I control the entire system with a uC and there aren't problem to reset the bq2002F in case of a temperature fault and understand when your…
Other Parts Discussed in Thread: BQ2002F
Hi.
I developed a battery chargers for 4 NiMh with BQ2002F (I saw and copied from the DV2002L2/T2 Dev. Kit)
It works perfectly. No problem.
But the Linear Regulator is very hot, so I'm thinking to replace with…
Other Parts Discussed in Thread: BQ2002F Hi Everyone,
I'm using the BQ2002F to charge a 2 series cells of NIMH battery. My Nimh Cell has 70 mAh as Nominal Capacity, and its manufacturer recommend to fast charging it using 35 mA for 3h (for fully discharged…
An addendum to my previous post:
Although the fix described above works, the battery is trickle charged at C/32, compared to the battery manufacturer's recommendation of C/300. This keeps the battery temperature about 5 0 C above ambient, which I suspect…
Other Parts Discussed in Thread: BQ2002F , BQ24105 I work in Optikon 2000 Spa (Italy) , a medical company and I use your BQ2002F in a footswitch (Bluetooth connection - battery supplied)
that is a part of ophthalmic surgical device .
Now I'm designing a…
Hi Chris, I did some tests in these days and I found that the battery pack wasn't 2100mAh but less...
I'm sorry.
The nominal capacity (for my manifacturer) is assured only if the cell is charged at c/10 for 16h and discharged at c/5.
A my…