Part Number: BQ2022A Other Parts Discussed in Thread: EV2400 Since EV2300 is not able to order now and TI suggest to use EV2400 work with bq2022A.
Is there any user's guide could share with how to programming bq2022A by EV2400? Thanks.
Part Number: BQ2022A Other Parts Discussed in Thread: MSP430AFE221 , Hi Expert,
My customer designed a bq2022A program board with MSP430AFE221 to program code for bq2022 . While they don't know what code they need to realize the programming function with…
Part Number: BQ2022Abq2022A datasheet specify SDQ pin programming voltage between 11.5V~12V, what is maximum voltage rating for SDQ pin? Since datasheet not mentioned about the maximum rating.
Part Number: BQ2022A Hello experts,
I got question about programming circuit example from customer.
Why do you set two 100 ohm resistors? Could you tell me the hardware setting point?
Also, I would appreciate if you would share me the additional material…
Part Number: BQ2022A Hi Support team
i have one question about Dell's PSID, how does the burning program read the PSID by burning tools? Will the way of reading be the same as the method on the system side?
Part Number: BQ2022A I am having some difficulties with the WRITE DATA MEMORY command.
I am using hardware that uses a UART with an open drain to generate the one wire signals.
I can issue the READ MEMORY/Page command successfully. I use the skip rom…
Part Number: BQ2022A Dear Sir.
As shown in the figure: The SDQ pin in the line has a 100R resistor. Please help confirm the following problem.
1. What is the specification of the resistance value range (minimum and maximum values) that the resistor R1…