Part Number: BQ24075 Other Parts Discussed in Thread: BQ24072 Tool/software: hi
Test charge protection time about BQ24072. The external power supply at the battery end is 3.8V, and the USB end is 5V. The battery is only connected to the NTC and GND to…
Part Number: BQ24075 Other Parts Discussed in Thread: TPS63061 Tool/software: Kindly review the schematic of Single cell Battery charger. You can ignore IP5306 circuit as it is not included in design. Basically We want to charge battery from USB-C and…
Part Number: BQ24075 Other Parts Discussed in Thread: BQ25170 , BQ25185 , BQ25710 , BQ25790 , BQ25180 Hi Team
do we have any batter charger IC for coin battery which can be conducted in shipping mode?
below is coin battery spec.
'
BRs
Brian
Part Number: BQ24075 in my application Vin =Vusb=5V for charging battery (1cell,4.2V,1000mAh) in case of deep discharge or low battery voltage the system should run in Vbus supply
is Vout 5.5V and Iout=4.5A available in below scenarios as per datashee…
Part Number: BQ24075 Other Parts Discussed in Thread: BQ25185 Hi,
1) The following thread discusses how to find battery connection/disconnection. In conclusion, what are the methods to find?
https://e2e.ti.com/support/power-management-group/power-management…
Part Number: BQ24075 Other Parts Discussed in Thread: BQ24230 , BQ24073 , BQ24074 Dear Mr./Mrs.:
I would like to know if the BQ24075 IC is a direct repalcement of the BQ24230 with PIN15 connected to VSS on both cases.
Many thanks in advanced
Part Number: BQ24075 Hello,
I have recently made a breakout board for the BQ24075RGTR chip.
To try it out, i connected all external components on a breadboard.
VBUS is a DC Power Supply which also displays the output current.
When i connect the battery…
Part Number: BQ24075 Adding to my previous question:
What is the IC's self current consumption when the input is disconnected (not charging the battery), and a 4.2V Li-ion battery is connected on the BAT pin? (The OUT pin is connected to a small capacitive…
Part Number: BQ24075 Hello,
the datasheet of the BQ24075 states that if I leave the TMR Pin unconnected the timers will be set to the default values.
Can you please tell me what the default values are and is it save to connect a battery with any capacity…
Part Number: BQ24075 Hey
Simple question, but something I can't see to confirm from the datasheet.
When the VIN voltage on the BQ24075 is at 5V. the battery is charging(4.2v li ion) and the out voltage is 5.5v.
When VIN is removed or below 5V the…