Part Number: BQ24075 Hi Experts, May I ask for help? By refering to the E2E post below: (1) BQ24075T: difference between BQ24075 & BQ24075T - Power management forum - Power management - TI E2E support forums Does it mean customer can use BQ24075TRGTT …
Part Number: BQ24075T Does the integrated circuit have an reverse battery voltage protection? So, what will be observed in OUT pin when battery is reversely put into this IC BATT pin?
Part Number: BQ24075T Other Parts Discussed in Thread: BQ24075 , Hi Team,
customer is wondering the difference between BQ24075 and BQ24075T and if we have any next gen solution based on these two parts for keyboard & mouse application?
Thanks!
Pat…
Part Number: BQ24075T Hi Sir,
Would you pls help for bq24075T schematic questions as below? thanks.
VIN: VBUS_CHG(5V), from USB
VBAT: 560mA, 1C Li-ion Polymer Cell, typ. 3.7V max 4.2V
Input Current set: 600mA
Output Current set: 556mA
Q:
EN2 connect…
Part Number: BQ24075T Other Parts Discussed in Thread: BQ24075 , BQ24232
Hello,
I am using the BQ24075T to charge a 320mA/h Lithium-ion Battery PACK whose datasheet states-: "Maximum charging current = 160mA".
The lowest fast charge current setting…
Part Number: BQ24075T Dear Sir,
I have a project need charge Li-ion battery, the Li-ion battery capacity is 2400mAh
I select use BQ24075T to charge it, and my settings are :
1.Fast charge current is 1.5A, the R(ISET)=604 ohm (1.47A).
2. Input current is…
Part Number: BQ24075T Other Parts Discussed in Thread: TPS61230A , BQ24072 , BQ24075 Hi,
I am using BQ24075T for single Li-Po 3.7V battery . The application is just it is like a battery bank for another single cell battery, I am using its power path Vout…
Part Number: BQ24075T Dear Sir,
I have a project need charge Li-ion battery, the Li-ion battery are 3 pcs parallel, the capacity is 4200mAh*3=12600mAh.
I select use BQ24075T to charge it, and my settings are :
1.Fast charge current is 1.4A, the R(ISET…
Part Number: BQ24075T
HI
We have a design that is using bq24075T as the charger.
There is a need to periodically check the voltage of the battery.
After we pull !CE high, took a ADC read and set !CE low (enable), we noticed that the charging does not…