Part Number: BQ24076 Other Parts Discussed in Thread: BQ25180 , The datasheet only states that bq24076 is capable of "5A" continuous current output but not the Rds(on) of internal battery FET. I am comparing it with the specifications in the bq25180 datasheet…
Part Number: BQ24076 Other Parts Discussed in Thread: BQ24072 , BQ24075 , BQ25180 I am using BQ24076RGTR. While charging the battery LED2 turning ON. I am using 3.7V nominal Li-Ion battery so It can go upto 4.2V. when bat voltage reached to 4.2,LED1 should…
Part Number: BQ24076 Other Parts Discussed in Thread: BQ24075 , , BQ24075T
Hi Sir,
As the title, Is BQ24076RGT compatible with BQ24075TRG? Due to BQ24075TRG is out of stock, so we would like to find a compatible device for the second choice. But BQ24076RGT…
Part Number: BQ24076 If I use battery can discharging 10A(more than 5A), May BQ24076CE cause damage? or May BQ24076CE work protective function (like OCP)?
I confirmed BQ24076CE's absolute maximum output current is 5A in datasheet.
Part Number: BQ24076 Other Parts Discussed in Thread: BQ24075-Q1 Hi team,
My customer is designing a charger topology for their automotive application.
They have some question about the bq24076 application as below. Sorry. Not very familiar with charger…
Part Number: BQ24076 Hi sir,
Understood that Bq2407x charger ic comes with internal short circuit protection when Vbat-Vout>0.25v,
Is there any method to disable the short circuit protection or increase the threshold?
Thanks
Part Number: BQ24076 I had similar issue which is not solved and meanwhile my client abandoned the project as his private issue. No I have new design, nee to power cellular modem powered 5-6V@1A solar panel outdoor use, during testing from PC USB connector…
Part Number: BQ24072 Other Parts Discussed in Thread: BQ24076 , BQ25886 , BQ24610 , BQ25606 , BQ25895
I have a few different PCB that contain several polymer battery types for same GSM module SIM800C. maximum voltage for module 4.4V above that voltage will…
Thank you Anthony for confirmation. After writing the whole below reply I realised that a wrong chip was used in production. It's BQ24076 which follows the battery voltage, not BQ24073. But I'm posting this anyway for anybody who would like to see how…
Part Number: BQ24076 Hello, I have a few questions regarding the BQ24076 Battery Charger.
1) What voltage battery can I use with this chip. The datasheet says V_bat is 4.4V, but I'm not sure if V_bat is the constraint on the battery voltage or the voltage…