Other Parts Discussed in Thread: BQ24095 Hi Sir
I have a question of BQ24095 could you hlep to explan, When battery absent (Battery detect mode), does system (OUT pin) current limit follow the Iset setting or just 10mA.
Part Number: BQ27441-G1 Other Parts Discussed in Thread: BQ24095 Hello Team,
We are working on one project and we selected bq27441-G1 fuel gauge for measurement of battery health & BQ24095 Charge controller for charging battery.
kindly review the attached…
Other Parts Discussed in Thread: BQ24095 Hi
Regarding BQ24095, we have some question.
1) BQ24095 connects system load and battery. BQ24095 charges the battery, and provide the power to system load as well.
At this condition, how does this device operate…
Other Parts Discussed in Thread: BQ24095 Hi,
I'm currently experiencing problems using the BQ24095 Ion charger.
Here's my circuit:
It looks like I followed the datasheet this way. R2 is not placed.
This is my layout:
There are two things which…
Other Parts Discussed in Thread: BQ24095 I designed a simple battery charger based on BQ24095.
Despite the fact that I sticked to the schematics found in the datasheet, the charger does not work.
Please see the schematic here below:
http://www.mdctechnology…
Other Parts Discussed in Thread: BQ24095 , BQ51050B Hi,
On single PCB, We have designed two options for 220mAh Li-Ion battery charging. (One with BQ24095 and another with BQ51050B)
we have limited fast charging current at 55mA in both the circuits by setting…
Hello Nick,
Okay. But we don't have 4.35V battery available right now. I checked same battery with BQ24095 IC and it's working fine. BQ24095 IC's specification is same and it is also give 4.35V as a output voltage.
Part Number: BQ24092 Other Parts Discussed in Thread: BQ24090 , BQ24091 , BQ24095 , BQ24093 Does BQ24092 conform to the JEITA specification?
Does TI have a specification for JEITA?
What does JEITA design need to be aware of?
Part Number: BQ24092 This part’s datasheet ( http://www.ti.com/lit/ds/symlink/bq24095.pdf) ., in pages 35 to 39 describes two different “Exposed Thermal Pad Dimensions” and corresponding examples of board layouts for the same part and package. Why…
Part Number: BQ24045 Other Parts Discussed in Thread: BQ24095 Hello
Do we have 4.35V charger solution that cost effective than BQ24045? Thank you.
BR
Patrick