Part Number: BQ24104 Other Parts Discussed in Thread: BQ24103 , Hello,
Our team is currently debugging our BQ24104 charger IC board. We are comparing our results with the data we got from the BQ24103 EVB. Here are our observations
A. With the 2S4P battery…
Other Parts Discussed in Thread: BQ24103 Hi,
I am using BQ24103 to charge a single cell Li Ion Battery. I need some clarifications regarding status pins.
Status pins from charger are taken to processor which shows the charging status on LCD based on status…
Other Parts Discussed in Thread: BQ24103 Hi,
We are using BQ24103 for battery charging. If the battery is absent VBAT falls between 0V and 4.2V.
Can we disable the battery detection circuit in this chip?
Please give me a solution as immediate as possible…
Other Parts Discussed in Thread: BQ24103 , STRIKE Hi,
I am using the typical 2-Cell 1.33A bq24103 charger aplication from datasheet.
One of our product was returned witch non functional charger - symptoms was:
Charging current = 5mA when Battery voltage…
Other Parts Discussed in Thread: BQ24103 Hai
My BQ24103 battery charging circuit is not working properly.
In this circuit battery is not charging please give a solution as immediate as possible
Now I am attaching my circuit
Regards
Binoy Johnson
…
Other Parts Discussed in Thread: BQ24103 We are using the TI BQ24103 Lion battery charging chip. I am using it on a test fixture in production that we use to test and condition batteries. It was originally configured with a TTC(time to charge) cap of 0…
Part Number: BQ24120 Other Parts Discussed in Thread: BQ24104 , BQ24109 , BQ24103 Can you confirm that the only difference between BQ24120 and BQ24104 are the following?
Pin 2 - STAT1 (behavior) - BQ24120 – either ON or OFF - BQ24104 – either ON or…