Part Number: BQ25303J Other Parts Discussed in Thread: BQ24105-Q1 Hi,
I'm using BQ25303J as battery charger in my design. But this part is not an automotive grade and operating Temp range in blw -40 to 85 degree Celsius.
Could you please suggest the…
Part Number: BQ24105-Q1 Dear team,
My customer is working on a PDC project. In this project, they need to charge the 12V main battery, so they need a charger device. The requirements are VIN=14.5V, VOUT=12V(VOUT_max=14V), I_charge_max=500mA. Is our device…
Part Number: BQ24105-Q1 Other Parts Discussed in Thread: BQ51013B , BQ25713 , BQ25710 Hi
I am designing a wireless charging system and a BQ51013B is used to regulate a 5V 1A and charge 3S 12.6V Li-ion battery. I think the output stage of the BQ24105-Q1…
Part Number: BQ24105-Q1 Hi,
1. Charging NIMH with bq24105-q1, 3 units in series with 1.2v, the theoretical calculation is 5.1v to charge the battery, but now it has been 4.6v, what is the possible reason?
2. Now the IC is charging the battery all the…
Part Number: BQ24079QW-Q1 Other Parts Discussed in Thread: BQ24105-Q1 Hi Team,
As title, I see the datasheet saying that the VBAT(REG) = 4.1V. Does it mean that the battery charger is only for 4.1V Battery?
If so, do we have automotive solution that…
Part Number: BQ26200 Other Parts Discussed in Thread: BQ24105-Q1 , BQ25171-Q1 , LM51231-Q1 Dear Team,
E-CALL has been evaluated to operate in an environment of -40 to 85 degrees Celsius. We will use nickel metal hydride battery pack. I hope the charging…
Part Number: BQ24105-Q1 Other Parts Discussed in Thread: BQ2000
Hi TI-team
My customer want to use BQ24105-Q1 for NiMH charging without using an external MCU.
Fig. 3 of the following document shows an example of NiMH charging using an external MCU.
…
Part Number: BQ24105-Q1 Hi TI-team
My customer have a question.
The maximum time that can be set in the data sheet is described as 572minutes (9.533 hours).
In "Charging NiMH Battery Using bq24105-Q1 in Automotive Applications", it is described as "It…
Part Number: BQ24105-Q1 Greetings,
I will select BQ24105-Q1 on my design.
My application is below 5.4V,
It should start charging,
I want to know how to set low voltage threshold,
For charging the battery.
Do I need to use any external component?
Any reference…