Part Number: BQ24125EVM-003 Other Parts Discussed in Thread: BQ24125 Hello,
I am planning to use BQ24125 Ic in my next project.
I just need some data.
My requirement : 3-cell Li-ion
Battery voltage range : 6V to 9V ,9Ah
Standard charging Current : 2 A …
There is only one EVM for this particular part. BQ24125EVM-003. I don't want to have to pay for yet another EVM so I will measure the characteristics on the custom units and post them.
Part Number: BQ24125 Dear TI community could you please review the schematic.
actually this is quite the same as reference design of bq24125EVM-003
I_charger = 0.23 A
U_charger = 12.6 V
Thanks a lot.
regards,
Mike