Part Number: BQ24130 Dear all,
I met a problem when using BQ24130 in charging for a Super capacitor.The output charging current does not meet the current I set. For example,when CMOD is set to low,and Viset2=2V, the sense resistor is set to 100mΩ,the…
Part Number: BQ25173 Other Parts Discussed in Thread: BQ51013B , BQ51013B-Q1 , BQ25171-Q1 , BQ24130 , BQ25170 , BQ51050B Hello Team, We plan to use the charger IC BQ25173 for one of our applications. Our requirements include a wireless supercapacitor charger…
Part Number: BQ24130 Other Parts Discussed in Thread: BQ24133
Hello,
Can you please advise if the below behavior is normal? Do we expect the output voltage to collapse with no cell connected? The status LED is telling me there is an issue:
The customer…
Part Number: BQ24130 Other Parts Discussed in Thread: BQ24171 , BQ24172 HI, is the BQ24130 able to charge a 3 cells 4.2V battery (max 12.6 V) with 12 V as PVCC ? If not, what is the minimum gap between PVCC and Vbatt ? Best regards
Part Number: BQ24130 Other Parts Discussed in Thread: BQ24133 My customer has a little problem with the charger: The LED1 is not turn off when the charge is complete.
Assembling of Liion batteries: 12.6В. At he end of the charging: Vin= 15.3 V Icharge =…
I am hosting a Raspberry PI computer and a 3 port USB-2.0 powered hub with the configuration. This will require about 1000 mAh current. I would like to know if this can be used to charge the batteries while in operation? I also need an LED indicator to…
Part Number: BQ24072T Other Parts Discussed in Thread: BQ24616 , BQ24130 Hello,
I want to use the BQ24072TRGTR Battery Charger IC to charge my LIPO battery 3.7V 6000mAh. I solely would like to supply power to my loads through the battery. Will not be using…
Other Parts Discussed in Thread: BQ24130BQ24130 has a CMOD pin to setup the precharge and fast charge current, I have a application is 1 cell battery charge. I want to the charger in pre-charge when the battery voltage is below 3V, and fast-charge when…