Other Parts Discussed in Thread: BQ24168 , BQ24160 Hello~
In the bq24168's datasheet, I found the table as below.
As I understand, "Charge current reduced by half" and "Charge voltage reduced by 140mV" mean the JEITA requirement. …
Other Parts Discussed in Thread: BQ24168 Support,
We have a customer usingt the BQ24168 and is having trouble with the I2C interface.
The symptom is read errors when the battery is charging. The errors occur at any data rate between standard mode (100kbps…
Other Parts Discussed in Thread: BQ24168 Hello~
As we know very well, BQ24168 is able to support JEITA.
But, in some cases, we just should be charging the battery between 0'C to 45'C temperature range, regardless of JEITA standard .
So I think as…
Other Parts Discussed in Thread: BQ24168 We have a customer that is not able to talk to the BQ24168 device reliably. Their clock speed is around 100 KHz. What is the min and max voltage for I2C signal 1.8 to 4.4 ? What is the recommended pull up resistor…
Other Parts Discussed in Thread: BQ24168 Hello~
Connect the AC adapter to system, and then when testing the experiment for remove & mount of the battery ( several times for short periods of time) , sometimes charger status does not return to normal from…
Hi Hp,
Unfortunately, there is no way for the user to disable the watchdog timer via I2C. There are two versions, BQ24160A and BQ24168 that have the watchdog and safety timers disabled. The table at the top of d/s page 4 shows the differences in the devices…
I would suggest using these. They are not hardware settable, but their default charge regulation voltage is 3.6V which is fine for your battery.
bq24160
bq24161
bq24163
bq24168
bq24261M
Regards,
Joel H
Other Parts Discussed in Thread: BQ24160A , BQ24161B , BQ24163 , BQ24168 , BQ24160 Dear all.
I'd like to confirm the contents of a datasheet. In the 9.3.14 External NTC Monitoring (TS), there is no mentioning of bq24160A in the following sentence.
"For…
Part Number: BQ24272 Other Parts Discussed in Thread: BQ24261M , , CC3100MOD , BQ24160 , BQ24168 Hello,
I have set the registers for 4.2 V operation. A lot of times the Battery OVP (overvoltage error occurs).
I would like to know at which battery voltage…