Part Number: BQ24196 I am using this BQ24196 to controlling an unexpected power interrupt, for that, I have used a 3.7V battery and my board running into 3.7V so when the power goes off I am running the device on the battery for 10 mins then after I was…
Part Number: BQ24196 Hi,
BQ24196 has connected to my board I2C line and my board is required to run 3.7V that's y I choose 3.7V battery. Here the condition is while board running time if any main power fluctuation gets it should be switchover from main…
Part Number: BQ24196 I have a requirement in which input is 5V, 3A, I need to have a LiIon battery backup. My output should be 3.3V for both conditions: 1) When I have input 5V supply 2) When I am running on battery
Can I use this part ? If yes, please…
Hi,
Below is the only sample driver available.
e2e.ti.com/.../faq-bq25890-could-ti-provide-the-sample-linux-driver-for-the-bq25890-bq25890h-bq25892-bq25895-bq25895m-bq25896-bq25898-bq25898d-bq24190-bq24192-bq24193-bq24195-bq24195l-bq24196-bq24295-bq24296m…
Part Number: TPS25948 Other Parts Discussed in Thread: BQ24196 , Tool/software: Good day,
We have a circuit board using the BQ24196 charger. We provide a 12V input and charge a single cell Li-ion battery.
As part of the safety tests, the input of the charger…
Part Number: BQ24196 Hi Sir,
Our customer used the BQ24196RGER for charger application, The RD setting Charge Voltage is 4.35V, But they are measure 4.1V discharge the battery.
Could you please support this issue?
Hugo
Part Number: BQ24196
BATFET_Disable it's not working. When i T urn off Q4 the entire board is getting OFF but its automatically getting ON after 50 seconds. What could be the issue?. How do i disable permanently until comes main power(adapter power…
Part Number: BQ24296 During charging, the led (connected to the STAT pin) started flashing at 1Hz which shows a charging problem. After disconnecting and reconnecting the charger, the led flashes faster.
Can this be related (as I read in a forum) to the…
Part Number: BQ24196 Other Parts Discussed in Thread: BQ24192 Sir,
I have connected 3.3V battery. when i was checked REG08[5:4] i am getting 10(it means fast charging)
even i checked REG01[5:4] i am getting battery is enabled(01). But why my battery is…