Part Number: BQ24232H Other Parts Discussed in Thread: BQ24232 , BQ25188 Tool/software: Hello,
For a small portable device I need to select a charger that could charge a 300mAH LiPol battery from a USB connector.
I need that the charger controller…
Part Number: BQ24232H Other Parts Discussed in Thread: BQ24232
Tool/software:
I'm working with a board that has a BQ24232H charger configured as follows:
R_Ilim = 5.1k R_Iset = 10k = Charge current should be ~88mA R_Iterm = 3.3k = Termination current…
Part Number: BQ24232H Other Parts Discussed in Thread: BQ24232 Hi team,
Does BQ24232 support dead battery, like this device working at Vbat = 0V? Like no battery present.
Part Number: BQ24232H Other Parts Discussed in Thread: BQ25185 , , , BQ24232 Tool/software: Hello guys,
One of my customers is looking for a Li-Ion battery charger like the follow.
1. Li-Ion 1S1P charging. 2. Standalone operation. 3. a charger which…
Part Number: BQ24232H HI Team,
is it possible to remove the external resistor at pin ILIM (pin 12) and let pin 12 not connected/floating, if this mode is not used mode (the intention is to use mode USB500mA, EN2 will be always connected to VSS/ground…
Part Number: BQ24232H Other Parts Discussed in Thread: BQ24040 , May I know what is the charging operation over TS? I can't find it in datasheet. Does it like BQ24040?
BR, Gary
Part Number: BQ24232H Other Parts Discussed in Thread: BQ24078 , BQ25606 , BQ25601 , Hi team,
My customer has another question on "precharge to fast-charge transition"
Please see the request from customer, thank you.
"
Because these 3 linear charger…
Part Number: BQ24232H Hi
We are planning to use BQ24232HRGTR battery charger. I have few query:
1. If battery voltage is let us day 3.3V and then we connected power adapter at input to charge the battery then what will be the battery charger output…
Part Number: BQ24232H
Hi, there,
I have a question regarding the temperature of charging.
According to IEC/EN 62368 (M.4) Li battery charging current shall not exceed its limit stated in battery spec. under different temperature. See below:…