Hello,
I would like to use the bq24260 for designing an inductive charger (alimented by USB), and I would like to know if this component supports small current for the fast charge (60 mA) ? My battery caracteristics : 3.7V 120mAh
Thank you for your…
Other Parts Discussed in Thread: BQ25896 we are looking for a form, fit, functional replacement for the BQ24260 VQFN package as the product page has it listed as not recommended for new design(NRFND). Specifically we looking direct replacement for a battery…
Other Parts Discussed in Thread: BQ25896 we are looking for a form, fit, functional replacement for the BQ24260 VQFN package as the product page has it listed as not recommended for new design(NRFND). Specifically we looking direct replacement for a battery…
Hi,
I am using BQ24260 for one of my projects.my device must work even without the battery(adapter only).
currently when no battery is connected, and while doing D+ D- checking,Vsys voltage is droping to less than 2v
this is causing to reset the…
Hi...
My customer is designing the application of battery charger.
And my customer is requesting the android driver of BQ24260.
Could I receive it?
If you have it, forward to me.
Thanks.
Other Parts Discussed in Thread: BQ24295 , BQ24296 I am looking for a form fit function replacement for the BQ24260 as the product page has it listed as NRND and the other parts in the family, according to the datasheet, do not have automatic USB detection…
I want to confirm bq24260 battery detection fuanction in the datasheet.
P18 8.4.6 Battery Detection
VDETECT = Vbatshort is correct?
VRCH is 120mV or Vbatreg - 120mV? (Vbatreg = 3.6V --> VRCH = 3.6V - 120mV = 3.48V?)
Best Regards.
Higa
Hi All,
I know that the recommended minimum inductor for bq24260 is 1.5uH but our customer hope to use it with 1uH to reduce footprint size. They understand and can accept higher inductor ripple current when smaller inductor is used. Can you accept…
I have a few questions about BQ24260.
1) There is a D+/D-_EN bit mentioned in the BQ24260 datasheet on page 20. But it does not appear in the register map. Is this register implemented, and if so, where is it in the register map?
2) Is there any problem…
Hi,
I am using BQ24260 for one of my projects. Currently when the device is on ,the battery regulation threshold is set as 4.2V and the watchdog is cleared every 15 seconds.but when the device is off ,watchdog timer will expire and BQ24260 will be in…