Part Number: BQ24259 Other Parts Discussed in Thread: BQ24296 Hello. I'm reading datasheets of bq24296 and bq24259 charger chips, and I don't see any differences. Is there any?
Best regards Piotr
Part Number: BQ24296 Hi,
I would like to get a design review of the charger section implemented.
We have a lithium ion battery with typical voltage 3.8V, max 4.2V and 2.2Ah. Trying to charge at 1C.
Here is the circuit:
Trying to send the board for…
Hi Star,
Please see my comments below.
Thank you for providing customer register read, but it does not provide all the answers, only that REG09 = 0x30 after reading twice. It would be best if customer could perform the following procedure and share the…
Part Number: BQ24296 Hi Dear,
The customer uses BQ24296. If the BQ24296 software is not configured and VBUS is powered normally, but there is no battery connected to the system, can VSYS output normally?
How can you tell from the Datasheet? The functional block diagrams for the 24295 vs the BQ24296 look basically identical. How about the BQ25616? Is the boost mode output to VBUS and PMID, or only to PMID?
Part Number: BQ24296 Hello,
I am working on a device that uses a BQ24296 charger to charge its internal Li-ion battery. The device draws current from a 24V car battery (through a step-down converter that feeds 5V into the charger's VBUS).
To protect…
Part Number: BQ24296 Hi There,
We are using BQ24296MRGER in our board for battery charging and we have observed that when we give the 3.0V from the battery the system voltage generates the 3.0V and we have observed that system voltage gives the same voltage…
Part Number: BQ24296 Hello Supporting Team, we are trying to implement a driver which is working with android 11, so far we managed to integrate the driver and to get the battery status and health, but we are not able to get the capacity, referring to…