Part Number: BQ24616 Tool/software: Hello team,
My customer is confused about the operating temp of this device.
On TI.com, opearating temp is -40 to 85 .
However, on datasheet, it is 0 to 125 .
Which statement is true?
If datasheet is true, then is…
Part Number: BQ24616 Other Parts Discussed in Thread: TPS25948 , Tool/software: Hello team,
What is the purpose of the input resistor and capacitor (R20 & C16)?
I am considering to use eFuse (TPS25948) before the back to back FET in the diagram below…
Part Number: BQ24616 Tool/software: Hi,
Thanks in advance,
We have already used BQ24616 in our old previous project where everything works all fine and good. We are using the same design in our new project also. but here the battery is not being charged…
Part Number: BQ24616 Hi Team. I had a few doubts and concerns regarding the BQ24616. We are developing a 6S charger using this IC and during testing ran into a few problems which led to the burnout of the IC itself. Aya Khedr was looking after my case…
Part Number: BQ24616 Tool/software: Hello I am currently designing a system using two batteries connected in series. The batteries each have their own built in NTCs (See product sheet attached). I am wondering if there are any proven solutions for letting…
Part Number: BQ24616 Hi, Customer wants to change charging profile, but not change IC. Charging temperature should follow IEC62133, or at least charging should be enabled between 10-45 degrees celcius. I am a bit confused about the bqstroller calculation…
Hi Effi,
I will close out this thread as I have not received an update.
Feel free to open a new thread if you have further questions.
Best Regards,
Aya Khedr
Part Number: BQ24616 Other Parts Discussed in Thread: BQ34Z100-G1 , BQ24610 Hi
The customer design with BQ34Z100-g1, the problem is can not charge full.
The schematic as below.
The red mark is the parameter changed, R9=5.6K, R10=16K. The circuit of BQ24610…
Part Number: BQ24616 Hi i would like to have my Bq24616 schematic and PCB reviewed. The board is without DPM enabled. I will share the files on private chat. Thanks and regards
Noel Binny Abraham