Part Number: BQ24616 Hello everyone ;
we are using BQ24616 to charge our battery to 16.8 volts from 17.5 power supply ;
in case there is no battery in the system ; battery is disconnected ; we see that BQ24616 is regulated the volt on the battery conenctor…
Part Number: BQ24616 Hi, my customer is facing the shutdown issue with the BQ24616.
____________________________________
We have not connected Battery thermistor to TS pin. So Resistors are adjusted to get around 2V input. But IC is disabling battery…
Part Number: BQ24616 Hi Team,
If my customer would like to charge the battery in the only 0~45C degree,
How to set RT1 and RT2? If they adjust R_HOT, how can find the resistor value for 45C?
Best Regards,
Austin
Part Number: BQ24616 Other Parts Discussed in Thread: BQ24650 , BQ24640 , We are planning to use the BQ2461x IC for a charger project that we have. We wanted to know something related to this IC. We are in need of an IC with very similar features that can…
Part Number: BQ24616 I am presently using, with success, the bq24616 to charge a 6S lithium battery at a maximum charge current of 3A. The voltage input into the system is typically 28V. To prevent any voltage spikes on the bus from damaging the bq24616…
Part Number: BQ24616 Hello team,
My customer asked me using C_ttc with 0.22uF on the TCC pin.
Is it okay to use 0.22uF?
According to datasheet, maximum t_charge is 10h, which means C_ttc should be less than 0.11uF. So, in my understanding, 0.22uF should…