Part Number: BQ24617 Dear Sir,
I am currently working on a new project that involves utilizing the BQ24617 for the pilot. However, I have encountered an issue where the quiescent current exceeds the specified 2mA mentioned in the datasheet. Upon further…
Part Number: BQ24617 Our device uses the BQ24617 charger with the TTC pin tied to ground through a 10kΩ resistor. It is my assumption that in this configuration, charge should never terminate. However I'm noticing a relatively rare situation where some…
Part Number: BQ24617 Hello
What should be the current setting for ACSET, when my system draws 4A and Battery charging setting is set to 3A.
Should I set it to 7A or only at 4A ?
Thanks
ATharva
Part Number: BQ24617 Hi,
I am using 3S Li-Po battery. It has two conenctors coming out.
One connector is A/K and second connector has charge balancing outputs for each cell.
How i can achieve balanced charge charging with BQ24617 ?
Thanks
ATharva
Part Number: BQ24617 Hi, I'm investigating a power path using bq24617, same as of bq2417x with 1-cell unremovable battery (SLUSAD2 Rev.C Figure.23).
System requirement: Vin =15 or 20V、Vbat = 12.6Vmax、Ichg = 1.5Amax
Is it possible to composite a charge…
Part Number: BQ24617 Other Parts Discussed in Thread: BQ29330 , , BQ29312A Hi,
In an upcomming project i want to use the BQ24617RGER and use this for a 4 cell lio-ion (in serie) pack. I'm planning to make a circuit with power path something like 10.2 typical…
Part Number: BQ24617 Other Parts Discussed in Thread: BQ24618 , , BQ24610 I'm having trouble procuring BQ24617 but can get BQ24610 or BQ24618. Is there a way to 'trick' these devices into working with the lower ACOV of 26V instead of 32V? I'm thinking a…
Part Number: BQ24610 Other Parts Discussed in Thread: BQ24617 , BQ24616 , , BQ24618 , BQ24630
Please see the below document for the layout guidelines and example for the BQ24610, BQ24616, BQ24617, BQ24618, and BQ24630.
Layout Guidelines and Example.pdf
Part Number: BQ24617 Hi, TI Support Team
The customer is trying to apply NTC to check the battery temp. using BQ24617.
The NTC stated in the datasheet recommends the use of 103AT, but the B value is not described.
Can you tell me about the B value?
…