Part Number: BQ24630EVM Hi,
I'm building charging circuit for LiFePo4 3-Cell (10.8V,16Ah with 2A charge rate) and I'm looking for BQ24630EVM Layout CAD files for reference purpose. Let me know where can i download the complete layout files.
…
Part Number: BQ24630EVM Other Parts Discussed in Thread: CSD18514Q5A Hello,
Can I test 10A charging current with BQ24630EVM?
If not, how can I test it?
What can I modify EVM to make to test 10A charging current?
Which components must be changed?
Could…
Other Parts Discussed in Thread: BQ24630EVM Is there a way to get the source schematic file for the BQ24630EVM pcb?
That should be included in the docs somewhere!
Other Parts Discussed in Thread: BQ24630EVM , BQ24630 Hi,
I am trying to use Bq24630EVM to charge an 8-cell LiFePO4 battery. I have multiple such batteries connected in parallel, and was trying to provide a 10A charging current. I am using a 28V/14A power…
Other Parts Discussed in Thread: BQ24630EVM , BQ24630 hello,
i use the bq24630 in my own layout and the bq24630EVM.
The Switching P-MOSFET i.e. bq24630EVM is a SI4401bdy and the controlvoltage from the bq24630 is 24V, but in the datasheet the recommended…
Other Parts Discussed in Thread: BQ24630 , BQ24630EVM Hi All,
This is my first time posting here and I am an amateur electronics enthusiast. Please forgive if I get some of the lingo wrong.
I am trying to fast charge 2 LiFE cells at 3.6 volts and 10 amps…
Other Parts Discussed in Thread: BQ24630EVM , BQ24630 Hello,
Are the Gerber files (or PDF's of them) and the BOM available for the BQ24630EVM LiFePO4 charger circuit?
I have designed a PCB with this chip but I can only get 80% effectiveness on my…