Part Number: BQ25125 Other Parts Discussed in Thread: BQ25120A , BQ25120F3A Hello,
In this thread BQ25125: BQ25125 IEC632368-1 CB Certification - Power management forum - Power management - TI E2E support forums you mention the IEC62368-1 CB Test certificate…
Part Number: BQ25120A Other Parts Discussed in Thread: BQ25125 , BQ25123 , BQ25121A , BQ25122 , BQ25120F3A
The devices BQ25120A, BQ25121A, BQ25122, BQ25123, BQ25125, etc., are all part of the same family of battery chargers: BQ25120x. They function similarly…
Part Number: BQ25120A Other Parts Discussed in Thread: BQ25121A , BQ25120F3A In microcontroller applications, the watchdog timer is use to assure the host is still responsive and have not stopped operating. The BQ25120A has a 50-s watchdog timer that monitors…
Part Number: BQ25120A Other Parts Discussed in Thread: BQ25125 , BQ25123 , BQ25122 , , BQ25121A , BQ25120F3A You cannot modify the default options of the device. After powering up or waking out of shipmode all registers will be set to default values. Any changes…
Hello Thomas,
We also have the bq25120f3a, section 6 of d/s has a most update to date comparison table comparing all the devices in this family: www.ti.com/.../bq25120f3a.pdf
Yes, recommend also getting an ev2400 to go along with the EVM. This is used…
Part Number: BQ25120A
The charger can enter shipmode by:
To enter shipmode on the BQ25120A, the device should be operating on battery-only mode (V IN < V UVLO ), and /CD and /MR must be high. Then you can:
Send the I2C command EN_SHIPMODE = 1 on the…
Part Number: BQ25120A The maximum discharge current you can pull from the PMID output depends on if adapter (VIN) is present or not. Operating on BAT only mode, the max current from PMID will be your Current Limit on Discharge Mode (IBAT_OCP). When the…
Part Number: BQ25120A The BQ25120A is a highly integrated power management unit which includes integrated power rails: a buck converter (SW/SYS) and a linear regulator (LDO/LS). The charger is also part of our power path family which includes the PMID…
Part Number: BQ25120A The BQ25120A implements a simple voltage battery monitor which can be used to determine the depth of discharge of your battery. A high-level representation of the circuit can be seen on Figure 17 of the datasheet. Table 2 provides…
Part Number: BQ25120A The dynamic power path management (DPPM) of the BQ25120A will separate the charging current from system current. When you have a valid IN source, current is shared at the PMID between charging the battery and providing system load…