Part Number: BQ25306 Tool/software: Hi,
I am using the BQ25306 IC to charge a 10,000mAh lithium polymer battery, and I need to set it up to charge at 3A. Based on the datasheet,
I understand the charge current ratio KICHGK_{ICHG} K I C H G and the relationship…
Part Number: BQ25306 Other Parts Discussed in Thread: BQ25638 , BQ25616 , BQ25606 Tool/software: Hello TI Team,
We intend to use battery charger IC in new upcoming product. For that, The BQ25306 is looks good but it does not have the USB detection option…
Part Number: BQ25306 Other Parts Discussed in Thread: BQ25798 Tool/software: Hello
I am using the BQ25306 to charge 2S1P LiFePo4 batteries.
in my nominal cases i have a fixed input voltgae of 12VDC
we are evaluating the possibility to use a A2V solar…
Part Number: BQ25306 Hello,
i am using the BQ25306 battery charging IC, i I designed the PCB according to the EVK, Please find the attachment inserted.
My question Is it possible to charge the micro-C-type USB with a VUSB with a 2A input on a VBAT 2-cell…
Part Number: BQ25306 Other Parts Discussed in Thread: BQ25886 , BQ25798 Hello Sir,
can we charge with input of 5v and the is battery of 8.4V Lipo.
if we want to charge with 5V VUSB charger with 1pack (4.2V Lipo) and 2 pack (8.4V Lipo)Cell?
and also, problems…
Part Number: BQ25306 Tool/software: I am not finding an explicit confirmation in the bq25306 datasheet that the STAT pin can be connected to a MCU GPIO with an internal pull-up. The reason I ask is that we are seeing the STAT pin glitch several times…
Part Number: BQ25306 Tool/software: Hi support team all.
I have a question about the STAT output when the battery is not connected. The conditions are as follows: - A circuit with the "power path" added as shown in Figure 10-8 on page 25 of the datasheet…
Part Number: BQ25306
Hi everyone,
I have question about BQ25306 for 2 cell battery charger. I designed circuit diagram, I totally followed datasheet of BQ25306 for the typical application (a standalone charger without power path) but it didn't charge…
Part Number: BQ25306 Dear TI Team:
I made the following standalone battery charger design using BQ25306:
The PCB design was as follows:
The PCB is functional, charges the battery completely and then the charger turns off until it detects low battery…