Part Number: BQ25306 Hi,
Could you please advise what configuration is suggested to implement the Battery remote sense for BQ25306?
VIN 9-17V
BAT=2S1P Li-Ion
VBAT_max=8.4V
Ich=2.5A
The battery pack is connected to a 1-meter cable, which has a typical impedance…
Thanks Garrett! I had already seen the application note you provided, it has a lot of very useful information, but it still has some limitation regarding the application I'm working on: - Linear charger BQ25173 seems great on a lot of points (including…
Part Number: BQ25306 Other Parts Discussed in Thread: BQ25300 , Hi everyone. I need some advice because I'm not very skilled about chargers.
I have two single cells (each with PCM). I have two possible technologies: either LiPo cells or either LiPO4 cells…
Part Number: BQ25306 Hello,
How can I skip the first two steps of trickle charge and pre-charge and start battery charging with the third fast charge step? If it's doable, could you provide me with the way to do it?
Best regards, Shinichi Yokota …
Part Number: BQ25306 1. Input power supply, solar panels. Specification: 9-12V/2A max
2. Charging voltage preset value 8.4V
3. Output is connected to the heating plate. Specification: 8-9V/500-800mA
The reason for using this chip as a DCDC is that relying…
Part Number: BQ25306 I am using bq25306 for charging a 7.4v battery. I have set the charging voltage to 8.4v .Resistor combination as per datasheet like 1.33M and 200k.
But the ic terminate the charging at 8.02v . The charging current I have set is 2…
Part Number: BQ25306 Other Parts Discussed in Thread: BQ24170 , BQ24610 , BQ25616 , BQ25886 , BQ24392 , BQ24171 Could you please suggest battery management IC which has following capabilities?
3/4A charging current
5 led indicators for battery charging status…
Part Number: BQ25306 Greetings:
We have been evaluating evaluation boards of BQ25306 (BMS005 Rev. A). We realized that there are two frequencies of LED's blinking periods when the power was turn on with a 2-cell battery: 1) 1Hz, 2) About 0.5Hz
…
Part Number: BQ25306 Hi TI Teams,
We have one question about the output voltage of the BQ25306, that is, whether the output voltage of the BQ25306 increases when the battery is in the protected state.
The battery that we used is a 7.4V lithium battery…