Part Number: BQ25302 Other Parts Discussed in Thread: BQ25303J , , BQ25306 , BQ25300 When battery is shorted, if the high-side FET (HSFET) of the charger turns on then there will be a direct low impedance path to GND resulting in high current through the…
Part Number: BQ25302 Other Parts Discussed in Thread: BQ25303J , , BQ25306 , BQ25300 The battery chargers BQ25300, BQ25302, BQ25306, BQ25303J control the charging enable and disable by the /EN and POL pins.
To enable charging, /EN and POL need to have opposite…
Part Number: BQ25306 Hi TI experts,
I implemented BQ25306 in our design, this ic according to the datasheet has a programmable charge voltage from 3.4V to 9.0V. In our design, the battery we use can be charge up to the max. continuous charging voltage…
Part Number: BQ25306 Other Parts Discussed in Thread: BQ25302 ,
Hi team,
1.I have noticed strange thing when battery is not connected with IC. Both battery and load is not connected --> Measured voltage across SW pins (inductor included) is ~4.15 Battery…
Part Number: BQ25306 Other Parts Discussed in Thread: TPS62136 , BQ24610 Hello everyone! I've got a three part question regarding Power Paths using the BQ25306. First, a little bit about my application:
Uses a Lithium Ion 2S4P battery: 8.4V, 8000m…
Part Number: BQ25306 Other Parts Discussed in Thread: BQ24610 , Dear TI:
I used a USB PD 3.0 Charger 60W to charge a Li-ion battery through BQ24610 and a USB PD controller IC.
Can I use one BQ25306 charge IC instead of BQ24610 and a USB PD controller IC…
Part Number: BQ25306 Hello all,
This is a follow up on a previous thread I posted about using a SPDT relay as a power path switcher for the BQ25306 charging IC, because the relay enabled a higher current to be passed on to the system compared to the 3A…
Part Number: BQ25306 Hello,
Is there a minimum value of output capacitance to keep the bq25306 stable?
We are using a 2.2uH inductor. 12Vin, 3.7Vout, 2.1A
Thank you, Keith
Part Number: BQ25306 Hi Team,
Customer is designing charger in he's project, and we have some question want to check.
Do we have a TS NTC calculator for BQ25306 at this moment?
Can we design the battery charging range in 0~50 degree C ? How to calculate…
Part Number: BQ25306 Other Parts Discussed in Thread: BQ24610 , BQ24650 Hi Team,
A customer would like to know if it is possible/allowed to use two BQ25306 in parallel in order to increase the charge current to 6A. If it is possible, can we just connect…