Part Number: BQ25306 Hello,
Is there a minimum value of output capacitance to keep the bq25306 stable?
We are using a 2.2uH inductor. 12Vin, 3.7Vout, 2.1A
Thank you, Keith
Part Number: BQ25306 Hi Team,
Customer is designing charger in he's project, and we have some question want to check.
Do we have a TS NTC calculator for BQ25306 at this moment?
Can we design the battery charging range in 0~50 degree C ? How to calculate…
Part Number: BQ25306 Other Parts Discussed in Thread: BQ24610 , BQ24650 Hi Team,
A customer would like to know if it is possible/allowed to use two BQ25306 in parallel in order to increase the charge current to 6A. If it is possible, can we just connect…
Part Number: BQ25306 When using the external power path topology circuit, is the 3A the total current including charge and system power? Or does it just represent the charge current only? Thanks! Lauren
Part Number: BQ25306 Other Parts Discussed in Thread: BQ25790 Hello expert,
My customer has one request ford charger and need to find solution to support 4.4V/3A charging voltage and current. They also need remote sense for voltage sense since they have…
Part Number: BQ25306 Following up from this previously posted question- https://e2e.ti.com/support/power-management/f/196/t/977787
Just to clarify, the input current regulation(I INDPM) is 3A min. So in a topology where I am powering the load through PMID…
Part Number: BQ25306 Hello TI team,
My customer is testing their own PCB with BQ25306.
I think the charging function works well so far, but the STAT pin is little strange.
when the battery pack is not attached in the system, STAT pin is not just low or…
Part Number: BQ294582 Other Parts Discussed in Thread: BQ25306 Hi team,
If the customer uses a 2pcs battery as a series and does not use BMS board.
I suggest customer use BQ294582+BQ25306 to design. It is okay for this?
simple blocks below.