Dear Ning Before I checked it once, I would like to ask you again about the termination current specifications of the BQ25611D. We need to know the following specification. [1] When BQ25611D detects COOL temp( T1~T2) with NTC, can BQ25611D detect termination…
Part Number: BQ25600D Other Parts Discussed in Thread: BQ24179 , BQ25600 Due to unavailability of parts, we switched from a BQ24179 to BQ25600 between revisions of our design. The original design with the 24719 showed very low radiated emissions when charging…
Part Number: BQ25600D Use the BQ25600D to manage/recharge the battery.
Noticed that when the battery was not used for a long time, plugging in the adapter (Output: 5V/3A or 9V/2A) does not exit the shipping mode.
However, it seems that an adapter with higher…
Part Number: BQ25600D Hi TI expert:
Our project will use charging IC BQ25600DYFFR with MT6371 for fast charging,
1. Please confirm whether this IC can adapt to MT6371 for fast charging scheme?
2. When using BQ25600DYFFR with MT 6371 for fast charging,how…
Part Number: BQ25600D Customer Question-
We have a housekeeping IC that can perform a hard reset. This IC currently outputs an active-high RESET signal for 1 second. When this signal is high, we expect all power sources to cut power to the system. When…
Other Parts Discussed in Thread: BQ25600 , BQ25601 , BQ25600C , BQ25600D , BQ25606 , BQ25601D
BQ2560x FAQ Home Page
This is the home page for common questions in relation to the BQ25600, BQ25600D, BQ25600C, BQ25601, BQ25601D, and BQ25606.
FAQs
Charge…
Part Number: BQ25601 Other Parts Discussed in Thread: BQ25619 , BQ25600 , , , BQ25600D , BQ25618E , BQ25618 , BQ25611D
The sample Linux driver for BQ25618, BQ25618E, BQ25619, BQ25611D, BQ25600, BQ25600D, BQ25601, BQ25601D is located here: www.ti.com/.../BQ256XXSW…
Part Number: BQ25618
The charger is basically a step-down DC-DC (buck) converter. It requires the input voltage to be higher than the output voltage with some headroom for normal operations.
The maximum duty cycle specification is one of the factors…
Part Number: BQ25618
When the input source is over-loaded, it is either from the current reaching the IINDPM (Input Current Limit) or from the voltage dropping to the VINDPM (Input Voltage Limit).
For the current to cause the input source to be overloaded…
Part Number: BQ25601
Due to the OTG boost mode’s startup delay, PMID voltage may dip for a short period after VBUS is removed. Check the charger’s corresponding datasheet for the specific timing of the device being used. In general, it is in the range…