Part Number: BQ25601D Hi Team,
just want to check if just BC1.2 function of BQ25601D is used and no charging function is used, how to config the part?
1. CE_N is pulled to GND
2. no external inductors and capacitors.
3. floating sys, bat
Thanks.
BRs
…
Part Number: BQ25601D Other Parts Discussed in Thread: BQ25618 , BQ25611D This device is used to charge batteries in the range 150 mAh to 2400 mAh. There is now a requirement to charge 45 mAh batteries but the lowest charge current and pre conditioning…
Hello Ning,
The customer wants to design Vth and Vtl, the calculation formula VREGN is to bring in 6V. But the customer actually took the BQ25601D evb to measure the VREGN voltage ① VBUS voltage is 5.0V~6.16V, VREGN voltage is VREG 4.99~6.159V, ② VBUS 6…
Part Number: BQ25601D Other Parts Discussed in Thread: BQ25601 , Hi team,
our customer plan to use BQ25601D to replace BQ25601 and can they leave the D+/D- floating to not use the function?
Hi,
Mr Jiju Chacko had a conf call with the TI field application engineer (FAE) and us this Tuesday. We have explained the charger operations and made some suggestions. Our FAE is working with Mr Jiju Chacko on the inquiry.
Thanks,
Ning.
Part Number: BQ25601D Other Parts Discussed in Thread: BQ25601 Hi Sir,
Does BQ25601 compatible with QC2.0? If not, can I know some charger IC that can replace it and support QC2.0.
Thanks,
Kind Reagrds
Part Number: BQ25601D Hi team,
For the BQ25601D, INT pulse notifies the system when input removed and the PG_STAT would goes to 0. My customer find that the PG_STAT is still 1 when the /INT occurs , so they want to know how long will it take from the…
Part Number: BQ25601 Other Parts Discussed in Thread: BQ25619 , BQ25600 , , , BQ25600D , BQ25618E , BQ25618 , BQ25611D
The sample Linux driver for BQ25618, BQ25618E, BQ25619, BQ25611D, BQ25600, BQ25600D, BQ25601, BQ25601D is located here: www.ti.com/.../BQ256XXSW…
Part Number: BQ25601D Hi team,
My customer wants to use BS25601D as below. Do you think there are any issues such the power ORing uses case?
Regards,
Takashi Onawa
Part Number: BQ25601D Other Parts Discussed in Thread: BQ24297 , Hi!
I am planning to replace BQ24297 with BQ25601D in current design. It seems HW plug and play instead of pins 10 (ILIM) and 8 (OTG). BQ25601D datasheet says leave these pins floating.
…