Part Number: BQ25611DEVM Tool/software: Hello, We are using the BQ25611D-EVM module. Can this EVM reliably detect OTG/Charger connections without fail? When connecting or disconnecting the charger, it detects correctly. However, it does not switch between…
Part Number: BQ25611DEVM Tool/software: Hi Ti, Does the OTG function of the BQ25611D-EVM only support OTG when it is in high mode, or can it support both OTG and USB charging simultaneously?
Part Number: BQ25611DEVM Other Parts Discussed in Thread: BQ25611D BQ25611DEVM development board test environment: 1. Power input VBUS 5V, 2. VBAT is not connected to the battery, 3. Connect the load to the VSYS end. Under the above test conditions, the…
Chris,
VSYS_min is valid when a valid adaptor is present. When in supplement mode with the battery only, VSYS follows VBAT. Please refer to 9.3.5.1 Narrow VDC Architecture and 9.3.5.3 Supplement Mode on the d/s for the details.
Thanks,
Ning
Part Number: BQ25611D Hello,
I am using the BQ25611DEVM for testing (no change in jumpers configuration) with benchtop power supply set to 5v 2A, connected to VIN (EVM J1)
The USB cable is disconnected
After powerup register 0x0 reads 0x4, I am…
Hello Ellie,
You can refer to the BQ25611DEVM and BQ25616 EVM user guide for the EVM schematic as reference. You will need external DC/DC or LDO for the 3.3V and 1.8V rail.
Yes, both device need MCU to control. MCU need to write to the BQ25611D or…
Part Number: BQ25611D Other Parts Discussed in Thread: , BQ25601D Hi team,
My customer has a couple of questions for a rather large project.
they only want to charge from all legacy USB ports (USB-C will be done with additional device). Now they…
Part Number: BQ25611D Other Parts Discussed in Thread: BQ25601D ,
I have a board, see attached screenshot of the power section, that originally had a BQ25601D but had to replace it with a BQ25611D due to the default over-voltage lockout setting of the…
Hi Gauthier,
Thank you for providing detailed information regarding the behavior you are observing.
I believe the STAT led blinking you are observing is the device transitioning back and forth between charging and not charging status. This is likely…