Part Number: BQ25628EVM Other Parts Discussed in Thread: EV2400 Tool/software: Hi,
I am currently working on bringing up this PMIC part. However, I am having some trouble maintaining the I2C connection after unplugging VBUS from the device while the…
Part Number: BQ25628EVM Other Parts Discussed in Thread: BQ25628 , Tool/software: Hi,
I am currently wrapping up the driver bringup for the BQ25628 PMIC and there are currently two issues that I would like to resolve.
1. I am using the BQ25628EVM…
Part Number: BQ25628EVM Other Parts Discussed in Thread: BQ25628 Hi
I have two questions about the BQ25628EVM's output without load.
1.The VBAT and VSYS waveform would keep VREGN for 50ms to 60ms when the system switch to charge status in no load…
Part Number: BQ25628EVM I use BQ25628EVM to test QON reset function and finding that it can be reset by QON only the BQ25628EVM in a non-charge state (without VBUS or disabling charge when VBUS exist). So, my question is can I reset the BQ25628EVM by…
Part Number: BQ25628EVM Other Parts Discussed in Thread: USB2ANY , EV2400 , BQSTUDIO Tool/software: We have ordered the BQ25628EVM for evaluation.
Jumper setup is as below.
The setup is as below.
We have used USB2Any interface board and the…
Part Number: BQ25628EVM Other Parts Discussed in Thread: BQSTUDIO , BQ25618 , BQ25628 , BQ25619 , EV2400 Dear Support,
I just bought the EVK mentioned in the subject and would like to use it with EV2400 & BQSTUDIO however the BQSTUDIO is not listing…
Part Number: BQ25628EVM Other Parts Discussed in Thread: BQSTUDIO , BQ25628 Hi,
When I got log from BQ25628 using BqStudio, is an interval of log fixed value ?
I set reading register interval in 1 second. But an interval of log was 4 seconds.
…