Part Number: BQ25758 Tool/software: Hi TI,
We are designing adaptor which can support Type-C Profile as below
5V, 9V, 12V, 15V, 20V, 28V, 36V, 48V This will support both EPR and SPR profiles
The maximum power is 240W (48V/5A).
We are using BQ25758 for…
Part Number: BQ25758 Other Parts Discussed in Thread: BQ25756 , BQ25750 , BQ25756E , LM5122 I am planning to use the BQ25758 in Buck mode for a bidirectional battery charger from 50V to 8V with charge current 5A and discharge current 50A. One limitation I…
Part Number: TPS25750 Other Parts Discussed in Thread: BQ25758 , TPS55288 , BQ25790 , BQ25713 , BQ25731 Hi,
Does TPS25750 can support PD3.0 DFP with BQ25758?
I've saw previous post said it can't support PD function with TPS55288. But don't know is it possible…
Part Number: BQ25720 Other Parts Discussed in Thread: BQ25758 Hi
My customer ask me, BQ25758 SW1 turns off every 40mS at bypass mode, is this normal?
The waveform as below
Part Number: BQ25720 Other Parts Discussed in Thread: BQ25758 Hi
There are two questions from customer about BQ25758 EPR power, I will send you detail via mail.
Can you help to provide the schedule of BQ25758 A2 ?
Is there any update about VBUS_LV circuit…
Hello Sumeet,
I will move to this thread to the DC/DC converter group.
By the way, if you need I2C control for your DC/DC converters, there is the BQ25758. The BQ25758 is a DC/DC converter that can output 0V to 60V at 20A.
Best Regards, Ethan Galloway …
Hi Rick,
The BQ2579x family is limited to 3.3A output in reverse/OTG/source mode so it is not able to utilize all of your 45-60W. For your power level, I recommend BQ25758, which is the BQ2575x dc/dc converter spin. Your 45-60W will connect to the BQ25758…
Hello Sankar,
Thanks for being patient with the delay. I was out of office Thursday and Friday.
We do not currently have a driver for the BQ25758. The BQ25758 and the BQ25756 have very similar registers. You should be able to modify the FreeRTOS BQ25…
Part Number: BQ25756 Other Parts Discussed in Thread: BQ25758 Tool/software: Application requirement:
DC side: DC 9V~60V
Battery Side:1~14cell LiOn battery
Mode:
1. Charger mode: 9~60V DC input, charge to 1~14cells battery, Charge current need to be…