Part Number: BQ25886EVM Hi Linhong,
My thread was locked.
This issue was not cleared. so I want to re-open and ask some question.
(+) BQ25886EVM: Input Current Limit by D+, D- - Power management forum - Power management - TI E2E support forums
How should…
Part Number: BQ25886EVM Other Parts Discussed in Thread: BQ25883 Hello Expert,
We are evaluating Input Current Limit (D+, D-, ILIM), Charging Current w/ BQ25886EVM.
Here is our setting.
-. Charging current : 1.3A
-. ILIM : 2.5A
-. connected the USB C-type…
Part Number: BQ25886EVM Hi, TI Application team,
is it possible to share me BQ25886EVM Altium design file? my email is don.chu@fleetwatch.com
Thank you
Don
Part Number: BQ25886EVM Other Parts Discussed in Thread: BQ25886 Hi,
My customer used BQ25886EVM but can't entry fast charge.
Our test condition as below.
1. Set ILIM to maximum.
2. Set ICHGSET to maximum.
3. Provide 5V to VBUS.
But battery charger…
Part Number: BQ25886EVM Hello Team,
My Customer is looking for the design files (Altium or CAD files) for BQ25886EVM. Is this available to be shared with them?
Regrads,
Renan
Part Number: BQ25886EVM Other Parts Discussed in Thread: BQ25886 , BQ25883 I've been evaluating the BQ25886 and noticed that the voltage seen by the battery pack (2S Li-Ion 2000mAh) is ~ 8.2 Volts when JP19 is connected (8.4 V). This voltage jumped up to…
Part Number: BQ25886EVM I am looking to evaluate the BQ25886EVM to charge a 2S 18650 Li-Ion battery pack. Upon reading through the spec sheet I noticed that it is suggested to use a battery simulator. My question is, is it required to use a battery simulator…
Part Number: BQ25886EVM Other Parts Discussed in Thread: BQ25886 , BQ25883 Hi,
When I charge a battery on the BQ25886-EVM to 8.4V (JP19 shorted), then discharge the battery to about 7.4V no-load. Then I switch the jumper to JP16 (8.2V charge voltage) and…
Part Number: BQ25886EVM Other Parts Discussed in Thread: BQ25886 I evaluating bq25886EVM on no battery connection, setting is nearly default and different points is below.
⇒ICHGSET: 1.5A, D+ and D- shorted (DCP), ILIM: two pattern for 1.5A and 2.5A, Battery…