Part Number: BQ25890 Hi,
We consider to use the dual BQ25890 for the one battery charge, and now, we plug in the Typc charger: without disconnecting the pogo charger R2059, the current detected by the battery pack IC is very different from the current…
Part Number: BQ25890
Hello TI Support Team,
We have a design that uses both the BQ25890 and BQ27546, and both devices have a dedicated thermistor (NTC) input.
We would like to confirm the recommended configuration for the thermistor connection when…
Part Number: BQ25890 Hi,
Plesae help to check the schematic diagram for BQ25890, and Why does GEGN (pin 22) have an output voltage when VBUS_POGO is not powered and the battery (CN2001) is connected? thanks.
Part Number: BQ25890 I am working on a design with a 3.7v Li Ion battery and a requirement for both 5v and 3.3v rails. But using the BQ25890 is causing extra problems because I am having to use both step up and step down subcircuits for these different…
Part Number: BQ25890 Hello,
Currently, we are working on a project, handheld product, and the battery charger and power supply section is devloped based on Texas parts. I have attached a schematic PDF file of our design for review.
Please review…
Part Number: BQ25890 Hi, I am working on a PCB that uses USB and is to be used in a final product at scale (using the BQ25890).
Because of this the capacitance on the VBUS line cannot exceed 10uF. In this case, it is recommended to use a 1uF capacitor…
Part Number: BQ25890 Other Parts Discussed in Thread: BQ25616 Hello,
I am using the BQ25890 for my design. My architecture would be as follows:
USB-C Receptacle
VBUS --------------------> BQ25890 VIN
D+ ----------------------> STM32 PA12 (USB…
Part Number: BQ25890 Tool/software: Hello
I am design a system that using the BQ25890 for the battery management. But I my CPU power up cuased by a power limited of the BQ25890.
The boards work fine for a PD power which can output 12V.
But it fail…
Part Number: BQ25890 Tool/software: As we know, for BQ25890,IINLIM or IDPM_LIM can be used by DPM. But what's the usage of ILIM pin controlled input current limit? That's to say if the input current limit of Charger is determined by ILIM pin, what will…
Part Number: BQ25890 Other Parts Discussed in Thread: BQ25895 Is it possible (when device isn't charging) to increase the voltage on the VSYS pin above the battery voltage.
We have a chip that has a minimum operating voltage of 3.6V connected to VSYS…