Part Number: BQ25895M We are currently designing a project based on the tablet. For that we are using bq25895m as the charging IC. For charging and data transfer USB-TYPE C connector is using in our designed schematics. Whether bq25895m supports USB-type…
Part Number: BQ25895M Other Parts Discussed in Thread: BQ25895 Schematics designed using BQ25895M charging IC is attached. Kindly go through it and let me know your comments.
VBUS power is connected to the power pin of USB C type connector. For passing…
Part Number: BQ25895M Other Parts Discussed in Thread: TS3USB221 , TUSB320 , , BQ25895 Kindly review the attached schematics designed using ICs BQ25895MRTWR, TS3USB221,TUSB320. Schematics is actually based on the battery charging and data transfer using USB…
Part Number: BQ25895M We are currently designing a schematics for a tablet project. USB C type charger is used for battery recharging and data transfer. And BQ25895m is used as charging IC. We are providing D+ and D- signals of USB connector directly…
Part Number: BQ25895 Hi,
I have an engineer using BQ25895 to replace BQ25895M in an existing design, and they're looking for a way to distinguish between the devices in firmware.
Looks like "Device Revision" in REG14 would be the right way to do that…
Part Number: BQ25895M Other Parts Discussed in Thread: BQ25895 Please help to check the operation behavior of BQ25895M
Boost mode operates when battery present and without any input source. Is it correct?
When input source plug in via VBUS(Assume 12V…
Part Number: BQ25895M Other Parts Discussed in Thread: BQ25890 Dear Sir,
We are testing OTG overcurrent limit and short to GND in boost mode.
but there are no protection for current limit and short.
I find just temperature protection for boost mode in…
Part Number: BQ25895M I really need to get past the glitch that occurs on PMID output, between the time that VBUS gets disconnected and the Boost Mode is operational. This seems to be at most a 30ms dip from about 5V to about Vbat, then back up to about…
Part Number: BQ25895M Other Parts Discussed in Thread: BQ25895 I'm using BQ25895M with an on-board 5V regulator providing power to the VBUS input (because outside voltage too high for BQ25895 as well as previous gen board using BQ24160R).
It keeps going…
Part Number: BQ25890 Other Parts Discussed in Thread: BQ25898 , BQ25896 , BQ25895 , BQ25898D , BQ25898C , BQ25892 , , , BQ25895M
Hi,
When only the battery is present, ADC monitoring works only when the battery voltage is above the MINSYS register setting. The…