Part Number: BQ25980 Other Parts Discussed in Thread: BQ25790 Tool/software: Dears,
one of my key customer is seeking for a high efficiency buck converter (Vin is 20~28V, Vout is half of the input voltage, iout max is 10A), the efficiency is expected…
Part Number: BQ25980 Other Parts Discussed in Thread: BQ25790 , Hi team,
My customer has a new phone project need 67W compatible 100W charging scheme.
Now they want to choose BQ25980+BQ25790 to realize.
Q1: Can BQ25980+BQ25790 meet this needs…
Part Number: BQ25980 Hi Team,
just want to check the spec on SDA settling time . There is no description on time spec of I2C in datasheet. Thanks.
BRs
Given
Part Number: BQ25890EVM-664 Other Parts Discussed in Thread: BQ25890
Now the /CE pin is connected full-down. I think we need to check if there is a pattern error related to heat dissipation in PCB artwork. When charging is continuously toggled, turn…
Part Number: BQ25980 Hi Team,
in datasheet, there are below conditions to turn on ACDRV.
regarding #6, if OVPFET is turn on, then Vbus should be above Vbus present. So how to understand #6? Thanks.
BRs
Given
Part Number: BQ25980 Other Parts Discussed in Thread: EV2400 Hi Team,
During test on below Iq_bat when adc is enabled, the result is above 1100uA which is beyond our spec.
for the 1st Iq_bat with ADC disabled, test result is ~22uA which is correct…
Part Number: BQ25980 Hi team,
BQ25980 is used for 2s battery charging, If the cost factor is not considered, can we use 1 BQ25980 as 2:1 to charge 1s battery?