Part Number: BQ27621-G1 Tool/software: Dear Team,
We are implementing the application code according to the following flow chart and after every reboot this application code runs which sets the data memory parameters.
We have also change the data…
Part Number: BQ27621-G1 Other Parts Discussed in Thread: BQ27427 , BQ27220
We have a single cell LiPo battery in our application and need to have fuel guage IC based on I2C.
We have shortlisted BQ27621, BQ27427 and BQ27220.
For all the 3 parts…
Part Number: BQ27621-G1 Tool/software: Hello,
In our sensor node project we shall use 3.6V Li-Ion battery pack which can be reach 17500mAh capacity. So we decided to use BQ27621-G1 as a battery fuel gauge IC. (For maximum capacity and compact design…
Part Number: BQ27621-G1 Other Parts Discussed in Thread: BQ27441-G1 Tool/software: Hi TI Team,
There are many system-side gauges for single cells, such as BQ27621-G1, BQ27441-G1 or etc.
Please provide information on the general functions and algorithms…
Part Number: BQ27621-G1 Tool/software: Hi team,
We have the request to implement by BQ27621YZFR-G1A. Please help us to know how to do the configuration to fulfill system spec.
1. Charge the battery by default current 0.5A or 0.9A. When the charging…
Part Number: BQ27621-G1 Other Parts Discussed in Thread: BQSTUDIO Hi Team,
I do have one query.
According to our battery parameters I do configure all necessary registers.
When the battery is charged to 4.2V and SOC is 100 percentage then I am seeing…
Part Number: BQ27621-G1 Tool/software: We plan to use the BQ27621 to measure battery voltage.
However, in some use cases, the battery connector may be connected to a 5V DC power source instead of a battery.
In this case, a voltage of about 5.0 to…
Part Number: BQ27621-G1 Other Parts Discussed in Thread: BQSTUDIO , BQ27Z561 , BQ27220 Tool/software:
Hello,
We are facing an issue with a battery powered device we are developing that utilizes a TI battery fuel gauge.
We are using a bq27621 fuel…
Part Number: BQ27621-G1 Other Parts Discussed in Thread: BQSTUDIO Tool/software: Dear TI team,
We are using IMX8M-mini to interface the the BQ27621 Fuel gauge. In our linux build using I2Ctool I do configure following register
Toggle Power Min,…
Part Number: BQ27621-G1 Hello,
Could you please help to chose a suitable Battery Gauge (Voltage based is prefered) for 18650/21700 LiNiCoAlO2 (NCA) Battery (like samsung 50E, Vapcell F56/F58/F60, LG M58T)?
Is it ok to use BQ27621-G1 with LiNiCoAlO2…