Part Number: BQ34110 Other Parts Discussed in Thread: GPCCEDV Hi, Our temp chamber would take weeks to arrive and we need to have the BQ34110 working even as not as accurate. can anyone share the CEDV profile of LifePo4 4S1P for BQ34110?
It would be better…
Part Number: BQ34110 Other Parts Discussed in Thread: EV2400 , BQSTUDIO Hello,
I am trying to run the GPC cycle for the BQ34110 (using the EVM and the EV2400). I have a 12V 6Ah LIFEPO4 battery. I followed the EVM tutorial and using a Digital load at 1.2Amps…
Part Number: BQ25172 Other Parts Discussed in Thread: BQ34110 ,
Hi,
The customer has used BQ25172 and BQ34110 for the design of charging and power monitoring. Since it is the first time to use them, please help review the schematic design.
Thank you…
Part Number: BQ34110 Other Parts Discussed in Thread: BQSTUDIO , , EV2400 Hello,
I'm having a failure "A read of data written failed comparison" when enabling VEN_EN bit or changing the flash update ok voltage.
I'm using a 4S Lifepo4, own…
Part Number: BQ34110 Other Parts Discussed in Thread: BQ35100 Dears,
Does BQ34110 supports Li-SOCl2 as BQ35100 supports it with chemID?
Is BQ34110's battery chemistry easily configured as BQ35100?
Kind regards,
Part Number: BQ34110 Other Parts Discussed in Thread: GPCCEDV Hello.
I am designing 6S7P BMS using BQ34110 Chip.
Cell setting and voltage calibration were performed by referring to "EV module user guide".
However, when discharging, the RSOC…
Part Number: BQ34110 Other Parts Discussed in Thread: GPCCHEM , GPCCEDV
Hello,
Can you tell which parameters of the screenshot below are per cell and which are for the entire pack ?
Currently, they are generated from the Excel file attached below.
But…
Part Number: BQ34110 I am trying to read the Manufacturer Information block registers of Fuel Gauge by sending the command "0x7000" from software. While reading the register, I am receiving only '0' even though as per the TRM it should be possible…
Part Number: BQ34110 Hi,
I was referring to the TRM of BQ34110 and it mentions(in section 4.3) that to unseal the device a unique set of two keys needs to be sent to the device via the Control() command.
May I know what is the default value of these…