Part Number: BQ40Z60EVM-578 Other Parts Discussed in Thread: BQ40Z60 Hello, everyone,
I wonder if the BTP function works correctly? Every time I connect the power supply on the evaluation board, the BTP-INT bit is set, even if the RSOC has 10% or higher…
Part Number: BQ40Z60EVM-578 Other Parts Discussed in Thread: BQ40Z60 , BQSTUDIO Hello,
I am unable to charge my battery pack.
I have attached the BQ40Z60 EVM's config file.
4S1P.gg.csv
Hello, I have already sent you the requested files (with other additional files). The attachments are in the post of Aug 12, 2020 10:11 AM. These correspond to my current configuration with the 200mohms shunt.
I hope I wouldn't be abandoned by TI's support…
Part Number: BQ40Z60EVM-578 Other Parts Discussed in Thread: BQ40Z60 , BQSTUDIO , EV2400 I'm working on BQ40Z60 battery management unit. The problem I'm facing is performing learning cycle on the board. While using BQstudio there on dashboard there is a…
Part Number: BQ40Z60EVM-578 Other Parts Discussed in Thread: BQ40Z60 Hello!
I use bq40z60 connected via SMBus to the Q7 processor module. The problem is that when i restart Windows 10, the bq40z60 battery stops seeing. I also have another laptop battery…
Part Number: BQ40Z60EVM-578 Other Parts Discussed in Thread: BQ40Z60 Hi together,
I'm trying to find out, if it is possible with the BQ40Z60 to have following behavior:
1. x seconds (wake) button pressed BQ40Z60 is wake up and activate XDSG and XCHG…
Part Number: BQ40Z60EVM-578 Other Parts Discussed in Thread: BQ40Z60 Hi there,
Steps that i have done:
choose the chemID 2059 for INR18650MJ1
configure the "Data Memory"
run the "Calibration" – Current Calibration and Voltage Calibration, Temperature…
Part Number: BQ40Z60EVM-578 Other Parts Discussed in Thread: BQSTUDIO , BQ40Z50-R1
Hi together,
1. My bqstudio show me in the Settings/Balancing Configuration different bits the are not mentioned in the manual. What does this bit do?
2. The CMB bit is …
Part Number: BQ40Z60EVM-578 Other Parts Discussed in Thread: BQ40Z60 I am working on BQ40Z60. When battery is not fully charged and the load is connected, at the same
time if suppose adapter is also connected. Will the adapter (charger) drive both the…
Part Number: BQ40Z60EVM-578 Other Parts Discussed in Thread: EV2400 , BQSTUDIO , GPCCHEM , BQ40Z60 Hello!
i am using qb40z60, ev2400 and battery robiton lp884765 (2-series) . When i run bqstudio, configurate necessery settings (DA settings, settings of charging…