Other Parts Discussed in Thread: BQ500511 , BQ50002 Hello,
is there maybe any product from TI, that offers Qi WPC compatible Wireless Power Transmitter logic and Power Stage in the same IC?
I do not want to use 2 big (48 or 64 pin; like BQ500511 and BQ50002…
Hi again. None of the mentioned TI transmitters are available: bq500212A bqTESLA Wireless Power TX EVM, nor bq50002 Wireless Power TX EVM, nor AVID FOD Transmitter. So we tried several combinations af Rfod and Ros at certification lab and found a pair which…
Thank you, I checked the BQ500212A EVM and then thought I'd look at other evaluation modules. What about the BQ50002 EVM (which uses the BQ500511)? I found it has an I2C interface which is apparently "used with bqStudio tool to monitor behavior" and…
Part Number: BQ500511A Other Parts Discussed in Thread: BQ500511 , BQ50002 , BQ50002A , Looking to use the bq500511 and bq50002 in a new design and I see the parts are flagged NRND. Are new parts in the works or should I look elsewhere ? Other solutions have…
Part Number: BQ500511 Other Parts Discussed in Thread: BQ50002 The problem occurs when I use bq50002EVM-607 or BQ500511+BQ50002:
After the battery is fully charged, the green LED on the power transmitter lights up:
And then, I repeat the following steps…
Other Parts Discussed in Thread: BQ500212A , BQ50002 , BQ500511 , BQ51051B Hello,
I'm at the beginning stages of a product, and I need a wireless charging solution, both Tx and Rx.
Tx: looking for <5W transmit
Rx: looking to charge a Li-Ion battery…
Thank you for your response. I understand that the frequency of BQ50002 is not fixed and can change based on some protocol.
My question is whether we can programmatically control the frequency in the user space. In my project, I have a MCU connected…
Part Number: BQ500511 Other Parts Discussed in Thread: BQ50002 , BQ501210 Is it possible to use the bq500511 alone (without a bq50002 or similar) with discrete power elements to achieve a higher power in the transfer?
Thanks in advance.
Other Parts Discussed in Thread: BQ500511A , BQ50002A , TIDA-00669 , TIDA-00623 , TIDA-00318 , BQ51013B , BQ51050B , BQ500212A , BQ24040 , BQ50002 , BQ500511 Hello All,
I am a newbee to wireless charging and I seriously need help. I have never worked on this kinda…