Other Parts Discussed in Thread: BQ500210bq500210 ES board is not work.
The switching frequency is written in the datasheet from 110KHz to 205KHz, but 60KHz is output.
ES circuit is attached. (and additional wire = 10 and 11pin 100K pull down to AGND…
Other Parts Discussed in Thread: BQ500210 Hi Sir
BQ500210 EVM of BOM show C15 and C13 the voltage rating is 100V from EVM BOM, does we can modify rating to 50V rating?
Other Parts Discussed in Thread: BQ500211 , BQ500210 , BQ51013A I would like to create a little wireless battery charger with input 5v.
My question is about the trasmitter. I have seen that bq55210 has input of 5V and bq500211 has 19V.
Can you explain me…
Other Parts Discussed in Thread: BQ500210 , BQ51013 I am trying to build a primary side using bq500210. I built the circuit according to the typical diagram in datasheet of bq500210, the one without MSPG2001. Now power regulator works well, giving a 3.3V…
Other Parts Discussed in Thread: BQ500210 , MSP430G2001 Hi,
We have made a Power transmitter based on bq500210. We are not (yet) using the MSP430G2001 and therefore the LEDs are directly connected to the bq500210. Our power transmitter works very well (tested…
Other Parts Discussed in Thread: BQ500210 , BQ51013 , BQ500410A Dear sir
I got Demon board of bq500210 & bq51013, we want to do modification of Demon board for multi coils transmitter.
Please provide som ideal to design the circuit.
Thank you very much…
Other Parts Discussed in Thread: BQ500210 We have based a PCB off of the Typical Application Diagram for Wireless Power Transmitter (Figure 7) in the bq500210 datasheet. The device analog pings but never detects a receiver when one is placed on the transmitter…
Other Parts Discussed in Thread: BQ500210 We have got questions about I2C and JTAG control from the customer.
1. Are there any fixtures for the connection and softwares for bq500210 you can provide?
2. What can we do with I2C of bq500210?
Best regards…
Hello Star
The HPA689 is our 19V input wireless power TX BQ500210 Evaluation board. This design uses the standard WPC A1 coil built by several manufactures.
One of them is Wurth Electronics, see P/N 760308101 for additional info.
Part Number: BQ500212A Other Parts Discussed in Thread: BQ51013B , BQ500210 , Hi team,
Our customer is reserching wireless power supply system.
I looked for Qi-compliant transmitter and receiver IC, and I found several receiver IC like BQ51013B.
I found…