Hello Wenjia,
I'm using TI's EVMs for both TX and RX. TX: BQ500410A RX:BQ51050B The LED D4 is in the transmitter. The input DC voltage is 12V and 500mA. Cheers,
Shruti
Other Parts Discussed in Thread: BQ500410A
Hi,
I have some issues building the circuit below. I have problems gettign teh TPS28225D to work properly. I am trying to build a wireless power transmitter, however, when i connect the transmitter coil…
Other Parts Discussed in Thread: BQ500410A The BQ500410A power stage is designed for 12V. ( WPC standard A6 )
Is it possible to use a single coil ( WPC standard A2, A3, A7, A15, A18 ) on BQ500410AEVM-085?
What should be changed in software and hardware…
I would recommend the bq500410A (12V) configured as a Single coil, data sheet figure 6.
The bq500410A can be configured with 1, 2 or 3 coils.
The bq500210 power section is designed to operate at 19V +/-1V. Conversion to 12V may be possible but there is…
Yes.
The single coil application circuit form the bq500410A can be used for power section. Rest of circuit will be from bq500412.
Yes Coil 1.2 and 1.3 drive signals will float.
We should have this fixed in a few days and the bq500412EVM-584 can be ordered through the TI eStore.
But bq500412 is a cost reduced version of the bq500410A. If you are evaluating wireless power transfer the older 410A has many of the same features. …
Other Parts Discussed in Thread: BQ500410A , BQ51050B Hello , I'm designing a battery charger complete with TX and RX using BQ500410A and BQ51050B for a lithium battery 2000mAh stylus. I made the coil transmit and receive because they have to be sma…
Other Parts Discussed in Thread: BQ500410A , BQ51051B , BQ51013B , BQ51050B Hello, I'm currently developing a project for my dissertation project and I was willing to use bq51013b, bq51050b, bq51051b and bq500410A, but in order to build my PCB, I found that…