Hello Bill,
Many thanks for your fast response and sorry for my late response. All of the information above is the details that I was looking for. I have another question, So I have this switch that when it gets activated the charging would start. I assume…
Part Number: BQ50002A Other Parts Discussed in Thread: BQ500511A ,
I'm currently using the BQ50002A and BQ500511A in a Qi transmitter design.
In the datasheet, there is a "Demodulator input signal conditioning" circuit.
This circuit takes…
Hello Metteo Pera
The BQ500511A has three settings that can be adjusted using external resistor, change voltage applied to pins.
1.) LED MODE -- Change LED behavior see data sheet table
2.) FOD_CAL -- This will change the shape of the loss curve vs…
Part Number: BQ500210 Other Parts Discussed in Thread: BQ51013A , BQ500511A , BQ51013B , BQ500212A Hi,
are the BQ500210 and the BQ51013A, EN303417 qualified? If not, do we have solutions that are?
Thank you, Stefan
Part Number: BQ51051B Other Parts Discussed in Thread: BQ500212A , BQ500511A , BQ50002A Hi Sir
if BQ51051B charge done
May I know TX board will indicate charge done or not ? or have any method can let TX board to know RX is going to charge done ?
Tha…
Hi,
I need to know if the BQ500511A and BQ50002A is available in your production for the 10 years on the futur?
Thank you for you answer.
Best regards.
Lionel
Operating freq cannot be controlled by I2C.
The bq50002A + bq500511A TX is an LLC resonant topology power converter, freq will change to meet output power requirements.
Part Number: BQ50002A Other Parts Discussed in Thread: BQ500511A , , TIDA-00623 I assembled a wireless power TX using the BQ50002A/BQ500511A as recommended on the BQ50002A datasheet (even though it recommends a 4-layer PCB I designed it with 2 layers) and…
Hi Wout
What is this 500ms cycling time you are talking about? ---Bill J -- The TX will turn off when it receives and End Power Transfer (EPT), the time it is off will depend on which EPT was sent. Charge complete is EPT01 and for the BQ500511A / 002A…