The thread listbq78350-R1A: " We have a design with AFE BQ76930 + gasGauge BQ78350-R1A with Fetdriver BQ76200."
Please specify the exact version that you use. I answered for the R1 version as listed in this thread.
Part Number: BQ78350-R1 Other Parts Discussed in Thread: BQ78350 , BQ76200 , BQ76940 , Tool/software: FAE, Hello! I have made a 14S lithium battery protection board using BQ78350-R1+BQ76940+BQ76200. Currently, I have produced 15pcs of samples, but 4pcs of…
Part Number: BQ76200 Tool/software: Dear Customer
Is the bq76200 resistant to radiation?
If not, please introduce me to a protection IC that can be used for space-related applications.
Thank you
Part Number: BQ76200 Other Parts Discussed in Thread: BQ76952 Tool/software: Hi Team, I am trying to understand the use of BQ76200 with multiple charge and discharge FETS. I have a few questions regarding it.
1) From the attached image, after reading…
Part Number: BQ76200 Tool/software: Can you confirm the chg/discharge/pchg FET can be enabled at the same time ?
I'd like to enable pchg FET for precharging capacitive load and subsequtenly enable the chg+dischg FETs simultaneously (without explicitly…
Part Number: BQ76200 Tool/software: We got a few BQ ICs implemented in our design at DoorDash Labs.
I would like to request a private sch review. Please reach out to me. Thx!
Part Number: BQ76200 Other Parts Discussed in Thread: BQ79656-Q1 , BQ79758-Q1 , , BQ76952 , BQ76940 Tool/software: Hi, I am trying to design a BMS with active cell balancing. TI team suggested BQ79656-Q1 (16S, 4th gen, does not require NDA for evaluation)…
Part Number: BQ76200 Tool/software: Design requirement High side NMOS drive tube opening time turn-off time is required within 50US, in order to do short circuit protection. 20 strings of 1 or 2 in parallel with 18650 batteries
Continuous current 100A…
Part Number: BQ76200 Other Parts Discussed in Thread: BQ78350 , , BQ76930 Tool/software: Hello,
I am having an issue with the BQ76200 coupled with the BQ76930 and BQ78350.
The problem that I have is that the power MOSFETs are not fully turning on as it…
Part Number: BQ76200 Other Parts Discussed in Thread: TPS4811-Q1
Tool/software:
I am using BQ76200 in my design currently for 48V system for driving MOSFET.
I want to replace Charge /Discharge MOSFET with Contactor for High current application. But I…