Part Number: BQ76920 Hello.
Below is the query related to BMS design using BQ76920.
On a manual press of reset button the requirement is to turn off the discharge FET by switching the BMS IC from Normal mode to Ship mode. To achieve this a voltage…
Part Number: BQ76920 Hello,
I have a BQ76920 set up fo 4 cell use. Cell 4 is the skipped cell. I'm testing at various discharge currents, and finding that after a higher amperage discharge (50A or higher in this case), cell 4 voltage that should be…
Part Number: BQ76920
Tool/software:
Hi team I have a 4s battery system with the BQ76920 as the BMS and VC3-VC4 shorted. However while reading the registers VC1 ... VC5, the VC4 register returns around 0.9V and the VC5 register returns 2.3XX V instead…
Part Number: BQ76920 Tool/software: Hi TI Team,
If the BQ76920 is used for 3 cells with the following schematic, what risks should I be aware of?
Will this cause any protections to be triggered?
Thanks!
Part Number: BQ76920 Hello,
I made a boneheaded error and didn't notice that SRP and SRN are reverse in my schematic of how The datasheet says to connect them. I have SRN connected to the GND/BATT- side of the sense resistor, and SRP to the DSG FET…
Part Number: BQ76920 Tool/software:
Hi,
Is it possible to disable under voltage protection for BQ76920?
We are expecting 0V on connected cell during certain operation.
Regards,
Ferlyn
Part Number: BQ76920 Hello,
We are currently developing a BQ76920 board and have encountered an issue regarding the Short Circuit in Discharge (SCD) fault.
During discharge, when a load of more than 1A is connected, the SCD fault triggers and…
Part Number: BQ76920 Tool/software: Hi Team,
Customer would like to know whether below register address of CB:6-10 and CB:11-15 is available in BQ76920? If not, when they write commend into these address in BQ76920, what will happen? They have 5s batteries…
Part Number: BQ76920 Tool/software:
Hi,teams!
Issue Description: During normal operation, the voltage of the second cell suddenly exhibits abnormally high voltage (around 9–10V) or abnormally low voltage (around 1–2V), while the expected…