Part Number: C2000WARE-MOTORCONTROL-SDK Other Parts Discussed in Thread: C2000WARE
Hi Experts,
Seeking your assistance as we have some points that need to clarify.
[1] As I understand it's a kind of firmware embedded inside some devices correctly? I am…
Yutaka Kamon said: ・1: Please explain why two events (CAU and PRD) are set for OutputA High and two events (CAD and ZRO) are set for OutputA Low.
Actually, only CAU and CAD will be triggered, and the other two events are just in case that a wrong value…
Part Number: C2000WARE-MOTORCONTROL-SDK Hello TI,
Can I use C2000 controller compiler with Code composer studio for commercial use?
We are using MATLAB for model based development and CC Studio for compiling and debugging the firmware.
Kindly let us…
Part Number: C2000WARE-MOTORCONTROL-SDK In the design that I'm working with, the current sense can put out a value corresponding to +400A at 5V to -400A at 0V.
For the "full scale" current value in this case, would it be the 400A, or the absolute…
Hello Shashank,
I figured there were some incorrect switch positions on the TMS320F280039C controlCARD and then after making the firmware changes in VBUS_CLK that you mentioned, it is working.
SFRA is now getting connected.
Thanks for the help and support…
Part Number: C2000WARE-MOTORCONTROL-SDK Other Parts Discussed in Thread: TMS320F28388D Hi,
I have a costumed deigned inverter with TMS320F28388D and a low inductance (28.5uH per phase), high speed (120,000RPM) PMSM motor. I am going to implement the sensor…
Hello Jason,
Sorry the forums went down and I was busy thoroughly examining all the configurations.
Jason Osborn said: Can you tell me the contents of the following ePWM registers, viewable in the CCS debug Registers or Expressions window?
EPWMx registers…
Part Number: C2000WARE-MOTORCONTROL-SDK I test the CCS project:is07_speed_control_coff,and see the the Clark transform as :
pOutVec->value[0] =((pInVec->value[0] *(float32_t)2.0f) - (pInVec->value[1] + pInVec->value[2])) * alpha_sf; pOutVec…
Part Number: TMS320F280049 Other Parts Discussed in Thread: C2000WARE
TI launchpad F280049, Code Composer Studio 9.0, C2000Ware 5.0, digital power SDK 5.0
I try to import the following project from digital power SDK.
When I try to build and load the…
Mitcham Tuell said: Further adjustments don't seem to give different outputs of motor ID other than making it not work at all. Do you think I need to continue tweaking them?
Just need to make sure that the motor run well without vibration and stop…