Part Number: CC1121 Hi team,
My customer faced with very rare issue with CC1121 when TX part of chip stops to work. The customer can't reproduce issue in lab, but already have tens of reports from their customers. Some customers never faced with the…
Part Number: CC1121 I would like to use the cc1121 transceiver in the 136-160MHz range (the datasheet sais “contact TI about it”). I also would like to use it in the 164-192MHz range. So my first question is - do i have to do anythig spacial to used in…
Part Number: CC1121 Other Parts Discussed in Thread: MSP430F5419A , CC1120 Hi ,
We are using MSP430F5419A with CC1121 in our Rf system, also we are using contiki2.7 OS.
The Contiki-conf file configurations are:
NETSTACK_CONF_MAC nullmac_driver
NETSTA…
Other Parts Discussed in Thread: CC1121 , CC1310 , CC1101 Hello!
We have to move fast from CC1121 to CC1310 radio, and we wonder is there a firmware for CC1310 who can work over SPI like a simple radio?
Best regards!
Part Number: CC1121 problem in the application of CC1121:
when a receiving device receives a plurality of data sent to the transmitting device, receiving device from the FIFO read out data there is crosstalk , the read data may be multiple packet combination…
Part Number: CC1121 Other Parts Discussed in Thread: CC1200 I plan to use the antenna diversity mode on the CC1121 transceiver. How can I determine which of the two antennas received the packet? I haven't an additional input to the microcontroller that…
Part Number: CC1121 Hello,
I have a customer who has a CC1121 configured with no sync word detect (SYNC_CFG0.SYNC_MODE = 0). Customer is trying to read FREQOFF_EST0 and FREQOFF_EST1 after a successful packet reception, but these registers are reading zero…
Part Number: CC1121 Other Parts Discussed in Thread: CC1101 Hello,
we have a project where we have to build a compatible CC1121 device which has to send some data to a old device with an CC1101 on it.
The communication is with ASK/OOK on 19.2kbps ins…
Part Number: CC1121 Hello,
I am trying to receive a packet of size 600 bytes with a baud rate of 100kbps.I configured my gpio2 interrupt to FIFO threshold (will get interrupt once in every100 bytes filed in fifo).When i was trying to read 100bytes immediately…
The TCXO looks ok as far as I can see from the datasheet.
Have you tried to measure the impedance on the non working board from every pin to ground and between every pin that could be in contact with each other (and compare with a know good board)?…