Part Number: CC1310 Tool/software: Hi
1. When using EasyLink application layer to send wireless data by calling EasyLink_transmit function, can you specify the total length of sending time, for example, fix a time node relative to the start of sending…
Part Number: CC1310 Tool/software: Hi ,
We see the following failure mode for a few of our CC1310 samples: The VDDR output fail to maintain the 1.68V when entering the deep-sleep mode. The VDDR gets few recharge pulses and then the voltage power down to…
Part Number: CC1310 Tool/software: i have a device with a cc1310 that transmits a signal to another device in 2 events. One event is when a car is detected, the other event is a timer that triggers every 7 seconds to alert the receiver device of its…
Part Number: CC1310 Tool/software: Hello
Is it possible to use this balun from TDK instead of the recommended ones (LFB18868MBG9E212 and 0850BM14E0016)?
They are compatible in terms of case size and pins.
Thanks for the reply.
rf_balun_hhm1776b3_en.…
Hi Yuning,
You can find details of the WB-DSSS mode here: SWRA591 ( Wide-Band DSSS Mode for FCC Digital Transmission Systems Using CC13x0 ) : https://www.ti.com/lit/swra591
From SWRA591, you would be most interested in Section 2 and 3 :
The SmartRF Studio settings…
Hi Yuning,
An example that may help clarify this, from https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/856174/ccs-launchxl-cc1350-rssi-to-dbm-equation-after-reading-from-register-0x4004-517c :
For the CC1310LP…
Part Number: CC1310 Tool/software: In my application i have 2 sensors connected to the same I2C bus. WHen i boot my device it initializes the I2C without errors but then when i try to write to one device the I2C just fails, this error is random since…
Hi Salih,
Do you have the possibility to provide a complete test project that reproduces the problem?
Alternatively, you can analyse the issue using ROV.
Regards,
Arthur
Part Number: CC1310 Tool/software: The CC1310 I use is connected to an external 24MHz crystal oscillator, not connected to a 32K crystal oscillator, the clock source configuration is 0x03, the SPI receiving packet data will be incomplete, and then the…