Part Number: CC2510-CC2511DK Hi, All!
I have CC2511 USB Dongle 1.3 and I have software SmartRF Flash Programmer, SmartRF Flash Programmer 2 and SmartRF Studio 7
I want to upload in CC2511 USB Dongle new firmware (sniffer_fw_ccxx11.hex). But my SmartRF Flash…
Part Number: CC2510 Other Parts Discussed in Thread: CC2511 , CC2340R5-Q1 , CC2340R5 We need low power SoC wireless transceiver with temperature
range from -55 to +125 deg C,
device like CC2510 is required,
small form factor device is required,
Please…
Part Number: CC2511 Hello together,
unfortunately I didn't found information in the datasheet how much current an GPIO pin can drive in low and/or high state.
i know the two pins with LED drive capability can drive a LED, but also unknown the value…
Part Number: CC2511 Other Parts Discussed in Thread: CC2510 Hello all,
The operating conditions for CC2511F32 is specified to work between 0°C and +85°C and between 3.0 V and 3.6 V.
What happened if temperature will be -25°C and / or the voltage…
Part Number: CC1110-CC1111 Other Parts Discussed in Thread: CC2511 We are utilizing the CC1110 as the SoC for our communication card on a CubeSat. We need to be able to flash the memory on the SoC with a hex file generated by us to run the communications…
Part Number: CC2511 Hi everyone,
I tried to convert the SWR85c sample from TI to Keil compiler. Without any success.
Has anybody a converted library for Keil ?
I want to transfer some data via virtual com port like serial interface.
Thanks a lot.
BR…
Part Number: CC2511 This dimension could be less vital to the antenna performance however I would like to follow the design. I can`t find it inside the reference document.
I have a CC debugger and two boards with CC2511F32 on them, I am running SmartRF Flash Programmer 1.12.7, the debugger is running firmware ID 05CC and the latest firmware which is 0041
The problem is I have a hex file that works on one board. I am trying…